Visitor II
Mar 3, 2023 1:03 AM UTC
Question
The STM32H743ZI's USB device virtual COM port (VCOM) with Free RTOS is broken after FW_H7 updating
- 2 replies
- 1208 views
The STM32H743ZI's USB device virtual COM port (VCOM) with Free RTOS is broken after updating to STM32CubeIDE v1.11.2. The problem is caused by FW_H7 updating from v1.10.0 to v1.11.0.
I have a program running on NUCLEO-H743ZI2 board. The USB device (VCOM) with Free RTOS works fine until STM32CubeIDE v1.11.2 update. The FW_H7 update from v1.10.0 to v1.11.0 broke the USB function. I can fix the problem by copying the old Driver\ fold over.
I think that the FW_H7_v1.11.0 has a bug in USB HAL library. Now I can only use the v1.10.0 and wait for fixing in the next release. I attached the .ioc file to help debugging.