cancel
Showing results for 
Search instead for 
Did you mean: 

STM32U585 + GPDMA +SPI +UART WORNG DATA

franckngatcha
Associate II

We're building a Wi-Fi gateway where the STM32U585 microcontroller communicates with a modem via both UART and SPI serial.

As for the serial port, we've configured it as follows:

void MX_USART1_UART_Init(void)
{

  /* USER CODE BEGIN USART1_Init 0 */

  /* USER CODE END USART1_Init 0 */

  /* USER CODE BEGIN USART1_Init 1 */

  /* USER CODE END USART1_Init 1 */
  huart1.Instance = USART1;
  huart1.Init.BaudRate = 115200;
  huart1.Init.WordLength = UART_WORDLENGTH_8B;
  huart1.Init.StopBits = UART_STOPBITS_1;
  huart1.Init.Parity = UART_PARITY_NONE;
  huart1.Init.Mode = UART_MODE_TX_RX;
  huart1.Init.HwFlowCtl = UART_HWCONTROL_RTS_CTS;
  huart1.Init.OverSampling = UART_OVERSAMPLING_16;
  huart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
  huart1.Init.ClockPrescaler = UART_PRESCALER_DIV1;
  huart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
  if (HAL_UART_Init(&huart1) != HAL_OK)
  {
    Error_Handler();
  }
  if (HAL_UARTEx_SetTxFifoThreshold(&huart1, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
  {
    Error_Handler();
  }
  if (HAL_UARTEx_SetRxFifoThreshold(&huart1, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
  {
    Error_Handler();
  }
  if (HAL_UARTEx_DisableFifoMode(&huart1) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN USART1_Init 2 */

  /* USER CODE END USART1_Init 2 */

}

void HAL_UART_MspInit(UART_HandleTypeDef* uartHandle)
{

  GPIO_InitTypeDef GPIO_InitStruct = {0};
  DMA_NodeConfTypeDef NodeConfig= {0};
  RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
 if(uartHandle->Instance==USART1)
  {
  /* USER CODE BEGIN USART1_MspInit 0 */

  /* USER CODE END USART1_MspInit 0 */

  /** Initializes the peripherals clock
  */
    PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART1;
    PeriphClkInit.Usart1ClockSelection = RCC_USART1CLKSOURCE_PCLK2;
    if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
    {
      Error_Handler();
    }

    /* USART1 clock enable */
    __HAL_RCC_USART1_CLK_ENABLE();

    __HAL_RCC_GPIOG_CLK_ENABLE();
    __HAL_RCC_GPIOB_CLK_ENABLE();
    /**USART1 GPIO Configuration
    PG11     ------> USART1_CTS
    PG12     ------> USART1_RTS
    PB6     ------> USART1_TX
    PB7     ------> USART1_RX
    */
    GPIO_InitStruct.Pin = CTS_WIFI_Pin;//CTS_WIFI_Pin|RTS_WIFI_Pin;
    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
    GPIO_InitStruct.Alternate = GPIO_AF7_USART1;
    HAL_GPIO_Init(GPIOG, &GPIO_InitStruct);

    GPIO_InitStruct.Pin = TX_W_IFI_Pin|RX_W_IFI_Pin;
    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
    GPIO_InitStruct.Alternate = GPIO_AF7_USART1;
    HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

    /* USART1 DMA Init */
    /* GPDMA1_REQUEST_USART1_RX Init */
    NodeConfig.NodeType = DMA_GPDMA_2D_NODE;
    NodeConfig.Init.Request = GPDMA1_REQUEST_USART1_RX;
    NodeConfig.Init.BlkHWRequest = DMA_BREQ_SINGLE_BURST;
    NodeConfig.Init.Direction = DMA_PERIPH_TO_MEMORY;
    NodeConfig.Init.SrcInc = DMA_SINC_FIXED;
    NodeConfig.Init.DestInc = DMA_DINC_FIXED;
    NodeConfig.Init.SrcDataWidth = DMA_SRC_DATAWIDTH_BYTE;
    NodeConfig.Init.DestDataWidth = DMA_DEST_DATAWIDTH_BYTE;
    NodeConfig.Init.SrcBurstLength = 1;
    NodeConfig.Init.DestBurstLength = 1;
    NodeConfig.Init.TransferAllocatedPort = DMA_SRC_ALLOCATED_PORT0|DMA_DEST_ALLOCATED_PORT0;
    NodeConfig.Init.TransferEventMode = DMA_TCEM_BLOCK_TRANSFER;
    NodeConfig.Init.Mode = DMA_NORMAL;
    NodeConfig.RepeatBlockConfig.RepeatCount = 1;
    NodeConfig.RepeatBlockConfig.SrcAddrOffset = 0;
    NodeConfig.RepeatBlockConfig.DestAddrOffset = 0;
    NodeConfig.RepeatBlockConfig.BlkSrcAddrOffset = 0;
    NodeConfig.RepeatBlockConfig.BlkDestAddrOffset = 0;
    NodeConfig.TriggerConfig.TriggerPolarity = DMA_TRIG_POLARITY_MASKED;
    NodeConfig.DataHandlingConfig.DataExchange = DMA_EXCHANGE_NONE;
    NodeConfig.DataHandlingConfig.DataAlignment = DMA_DATA_RIGHTALIGN_ZEROPADDED;
    if (HAL_DMAEx_List_BuildNode(&NodeConfig, &Node_GPDMA1_Channel15) != HAL_OK)
    {
      Error_Handler();
    }

    if (HAL_DMAEx_List_InsertNode(&List_GPDMA1_Channel15, NULL, &Node_GPDMA1_Channel15) != HAL_OK)
    {
      Error_Handler();
    }

    if (HAL_DMAEx_List_SetCircularMode(&List_GPDMA1_Channel15) != HAL_OK)
    {
      Error_Handler();
    }

    handle_GPDMA1_Channel15.Instance = GPDMA1_Channel15;
    handle_GPDMA1_Channel15.InitLinkedList.Priority = DMA_LOW_PRIORITY_LOW_WEIGHT;
    handle_GPDMA1_Channel15.InitLinkedList.LinkStepMode = DMA_LSM_FULL_EXECUTION;
    handle_GPDMA1_Channel15.InitLinkedList.LinkAllocatedPort = DMA_LINK_ALLOCATED_PORT0;
    handle_GPDMA1_Channel15.InitLinkedList.TransferEventMode = DMA_TCEM_BLOCK_TRANSFER;
    handle_GPDMA1_Channel15.InitLinkedList.LinkedListMode = DMA_LINKEDLIST_CIRCULAR;
    if (HAL_DMAEx_List_Init(&handle_GPDMA1_Channel15) != HAL_OK)
    {
      Error_Handler();
    }

    if (HAL_DMAEx_List_LinkQ(&handle_GPDMA1_Channel15, &List_GPDMA1_Channel15) != HAL_OK)
    {
      Error_Handler();
    }

    __HAL_LINKDMA(uartHandle, hdmarx, handle_GPDMA1_Channel15);

    if (HAL_DMA_ConfigChannelAttributes(&handle_GPDMA1_Channel15, DMA_CHANNEL_NPRIV) != HAL_OK)
    {
      Error_Handler();
    }

    /* GPDMA1_REQUEST_USART1_TX Init */
    handle_GPDMA1_Channel14.Instance = GPDMA1_Channel14;
    handle_GPDMA1_Channel14.Init.Request = GPDMA1_REQUEST_USART1_TX;
    handle_GPDMA1_Channel14.Init.BlkHWRequest = DMA_BREQ_SINGLE_BURST;
    handle_GPDMA1_Channel14.Init.Direction = DMA_PERIPH_TO_MEMORY;
    handle_GPDMA1_Channel14.Init.SrcInc = DMA_SINC_FIXED;
    handle_GPDMA1_Channel14.Init.DestInc = DMA_DINC_FIXED;
    handle_GPDMA1_Channel14.Init.SrcDataWidth = DMA_SRC_DATAWIDTH_BYTE;
    handle_GPDMA1_Channel14.Init.DestDataWidth = DMA_DEST_DATAWIDTH_BYTE;
    handle_GPDMA1_Channel14.Init.Priority = DMA_LOW_PRIORITY_LOW_WEIGHT;
    handle_GPDMA1_Channel14.Init.SrcBurstLength = 1;
    handle_GPDMA1_Channel14.Init.DestBurstLength = 1;
    handle_GPDMA1_Channel14.Init.TransferAllocatedPort = DMA_SRC_ALLOCATED_PORT0|DMA_DEST_ALLOCATED_PORT0;
    handle_GPDMA1_Channel14.Init.TransferEventMode = DMA_TCEM_BLOCK_TRANSFER;
    handle_GPDMA1_Channel14.Init.Mode = DMA_NORMAL;
    if (HAL_DMA_Init(&handle_GPDMA1_Channel14) != HAL_OK)
    {
      Error_Handler();
    }

    __HAL_LINKDMA(uartHandle, hdmatx, handle_GPDMA1_Channel14);

    if (HAL_DMA_ConfigChannelAttributes(&handle_GPDMA1_Channel14, DMA_CHANNEL_NPRIV) != HAL_OK)
    {
      Error_Handler();
    }

    /* USART1 interrupt Init */
    HAL_NVIC_SetPriority(USART1_IRQn, 0, 0);
    HAL_NVIC_EnableIRQ(USART1_IRQn);
  /* USER CODE BEGIN USART1_MspInit 1 */

  /* USER CODE END USART1_MspInit 1 */
  }
 
 
}

void HAL_UART_MspDeInit(UART_HandleTypeDef* uartHandle)
{

  if(uartHandle->Instance==LPUART1)
  {
  /* USER CODE BEGIN LPUART1_MspDeInit 0 */

  /* USER CODE END LPUART1_MspDeInit 0 */
	if(uartHandle->Instance==USART1)
  {
  /* USER CODE BEGIN USART1_MspDeInit 0 */

  /* USER CODE END USART1_MspDeInit 0 */
    /* Peripheral clock disable */
    __HAL_RCC_USART1_CLK_DISABLE();

    /**USART1 GPIO Configuration
    PG11     ------> USART1_CTS
    PG12     ------> USART1_RTS
    PB6     ------> USART1_TX
    PB7     ------> USART1_RX
    */
    HAL_GPIO_DeInit(GPIOG, CTS_WIFI_Pin|RTS_WIFI_Pin);

    HAL_GPIO_DeInit(GPIOB, TX_W_IFI_Pin|RX_W_IFI_Pin);

    /* USART1 DMA DeInit */
    HAL_DMA_DeInit(uartHandle->hdmarx);
    HAL_DMA_DeInit(uartHandle->hdmatx);

    /* USART1 interrupt Deinit */
    HAL_NVIC_DisableIRQ(USART1_IRQn);
  /* USER CODE BEGIN USART1_MspDeInit 1 */

  /* USER CODE END USART1_MspDeInit 1 */
  }
  

}

When used in interrupt mode, everything works fine.When used in interrupt mode, I cannot increase the baud rate because after a while the application crashes due to too many interrupts,  But when I receive in DMA mode, after a few characters are received correctly, it starts receiving the same character over and over again. It's in the buffer, and I don't understand what could be causing it. The same thing happens if I use the SPI + DMA serial port to communicate with the modem.

Catturauart.PNG

As you can see from the image, the first characters are correct. The interrupts arrive fine, but the buffer is incorrect. Always repeat the last correct character. The same thing happens if I read the data with the SPI peripheral; it just happens a little less frequently.It should be noted that here too I have to lower the clock frequency considerably so that this happens less often, compromising the communication speed during operations such as file downloads.

/* SPI3 init function */
void MX_SPI3_Init(void)
{

  /* USER CODE BEGIN SPI3_Init 0 */

  /* USER CODE END SPI3_Init 0 */

  SPI_AutonomousModeConfTypeDef HAL_SPI_AutonomousMode_Cfg_Struct = {0};

  /* USER CODE BEGIN SPI3_Init 1 */

  /* USER CODE END SPI3_Init 1 */
  hspi3.Instance = SPI3;
  hspi3.Init.Mode = SPI_MODE_MASTER;
  hspi3.Init.Direction = SPI_DIRECTION_2LINES;
  hspi3.Init.DataSize = SPI_DATASIZE_8BIT;
  hspi3.Init.CLKPolarity = SPI_POLARITY_HIGH;
  hspi3.Init.CLKPhase = SPI_PHASE_1EDGE;
  hspi3.Init.NSS = SPI_NSS_SOFT;
  hspi3.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_64;
  hspi3.Init.FirstBit = SPI_FIRSTBIT_MSB;
  hspi3.Init.TIMode = SPI_TIMODE_DISABLE;
  hspi3.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
  hspi3.Init.CRCPolynomial = 0x7;
  hspi3.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;
  hspi3.Init.NSSPolarity = SPI_NSS_POLARITY_LOW;
  hspi3.Init.FifoThreshold = SPI_FIFO_THRESHOLD_01DATA;
  hspi3.Init.MasterSSIdleness = SPI_MASTER_SS_IDLENESS_00CYCLE;
  hspi3.Init.MasterInterDataIdleness = SPI_MASTER_INTERDATA_IDLENESS_00CYCLE;
  hspi3.Init.MasterReceiverAutoSusp = SPI_MASTER_RX_AUTOSUSP_DISABLE;
  hspi3.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_DISABLE;
  hspi3.Init.IOSwap = SPI_IO_SWAP_DISABLE;
  hspi3.Init.ReadyMasterManagement = SPI_RDY_MASTER_MANAGEMENT_INTERNALLY;
  hspi3.Init.ReadyPolarity = SPI_RDY_POLARITY_HIGH;
  if (HAL_SPI_Init(&hspi3) != HAL_OK)
  {
    Error_Handler();
  }
  HAL_SPI_AutonomousMode_Cfg_Struct.TriggerState = SPI_AUTO_MODE_DISABLE;
  HAL_SPI_AutonomousMode_Cfg_Struct.TriggerSelection = SPI_GRP2_LPDMA_CH0_TCF_TRG;
  HAL_SPI_AutonomousMode_Cfg_Struct.TriggerPolarity = SPI_TRIG_POLARITY_RISING;
  if (HAL_SPIEx_SetConfigAutonomousMode(&hspi3, &HAL_SPI_AutonomousMode_Cfg_Struct) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN SPI3_Init 2 */

  /* USER CODE END SPI3_Init 2 */

}

void HAL_SPI_MspInit(SPI_HandleTypeDef* spiHandle)
{

  GPIO_InitTypeDef GPIO_InitStruct = {0};
  RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
  if(spiHandle->Instance==SPI1)
  {
  /* USER CODE BEGIN SPI1_MspInit 0 */

  /* USER CODE END SPI1_MspInit 0 */

  /** Initializes the peripherals clock
  */
    PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_SPI1;
    PeriphClkInit.Spi1ClockSelection = RCC_SPI1CLKSOURCE_SYSCLK;
    if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
    {
      Error_Handler();
    }

    /* SPI1 clock enable */
    __HAL_RCC_SPI1_CLK_ENABLE();

    __HAL_RCC_GPIOG_CLK_ENABLE();
    /**SPI1 GPIO Configuration
    PG2     ------> SPI1_SCK
    PG3     ------> SPI1_MISO
    PG4     ------> SPI1_MOSI
    */
    GPIO_InitStruct.Pin = FL1_SCK_Pin|FL1_SO_Pin|FL1_SI_Pin;
    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
    GPIO_InitStruct.Alternate = GPIO_AF5_SPI1;
    HAL_GPIO_Init(GPIOG, &GPIO_InitStruct);

    /* SPI1 DMA Init */
    /* GPDMA1_REQUEST_SPI1_RX Init */
    handle_GPDMA1_Channel13.Instance = GPDMA1_Channel13;
    handle_GPDMA1_Channel13.Init.Request = GPDMA1_REQUEST_SPI1_RX;
    handle_GPDMA1_Channel13.Init.BlkHWRequest = DMA_BREQ_SINGLE_BURST;
    handle_GPDMA1_Channel13.Init.Direction = DMA_PERIPH_TO_MEMORY;
    handle_GPDMA1_Channel13.Init.SrcInc = DMA_SINC_FIXED;
    handle_GPDMA1_Channel13.Init.DestInc = DMA_DINC_FIXED;
    handle_GPDMA1_Channel13.Init.SrcDataWidth = DMA_SRC_DATAWIDTH_BYTE;
    handle_GPDMA1_Channel13.Init.DestDataWidth = DMA_DEST_DATAWIDTH_BYTE;
    handle_GPDMA1_Channel13.Init.Priority = DMA_LOW_PRIORITY_LOW_WEIGHT;
    handle_GPDMA1_Channel13.Init.SrcBurstLength = 1;
    handle_GPDMA1_Channel13.Init.DestBurstLength = 1;
    handle_GPDMA1_Channel13.Init.TransferAllocatedPort = DMA_SRC_ALLOCATED_PORT0|DMA_DEST_ALLOCATED_PORT0;
    handle_GPDMA1_Channel13.Init.TransferEventMode = DMA_TCEM_BLOCK_TRANSFER;
    handle_GPDMA1_Channel13.Init.Mode = DMA_NORMAL;
    if (HAL_DMA_Init(&handle_GPDMA1_Channel13) != HAL_OK)
    {
      Error_Handler();
    }

    __HAL_LINKDMA(spiHandle, hdmarx, handle_GPDMA1_Channel13);

    if (HAL_DMA_ConfigChannelAttributes(&handle_GPDMA1_Channel13, DMA_CHANNEL_NPRIV) != HAL_OK)
    {
      Error_Handler();
    }

    /* GPDMA1_REQUEST_SPI1_TX Init */
    handle_GPDMA1_Channel0.Instance = GPDMA1_Channel0;
    handle_GPDMA1_Channel0.Init.Request = GPDMA1_REQUEST_SPI1_TX;
    handle_GPDMA1_Channel0.Init.BlkHWRequest = DMA_BREQ_SINGLE_BURST;
    handle_GPDMA1_Channel0.Init.Direction = DMA_PERIPH_TO_MEMORY;
    handle_GPDMA1_Channel0.Init.SrcInc = DMA_SINC_FIXED;
    handle_GPDMA1_Channel0.Init.DestInc = DMA_DINC_FIXED;
    handle_GPDMA1_Channel0.Init.SrcDataWidth = DMA_SRC_DATAWIDTH_BYTE;
    handle_GPDMA1_Channel0.Init.DestDataWidth = DMA_DEST_DATAWIDTH_BYTE;
    handle_GPDMA1_Channel0.Init.Priority = DMA_LOW_PRIORITY_LOW_WEIGHT;
    handle_GPDMA1_Channel0.Init.SrcBurstLength = 1;
    handle_GPDMA1_Channel0.Init.DestBurstLength = 1;
    handle_GPDMA1_Channel0.Init.TransferAllocatedPort = DMA_SRC_ALLOCATED_PORT0|DMA_DEST_ALLOCATED_PORT0;
    handle_GPDMA1_Channel0.Init.TransferEventMode = DMA_TCEM_BLOCK_TRANSFER;
    handle_GPDMA1_Channel0.Init.Mode = DMA_NORMAL;
    if (HAL_DMA_Init(&handle_GPDMA1_Channel0) != HAL_OK)
    {
      Error_Handler();
    }

    __HAL_LINKDMA(spiHandle, hdmatx, handle_GPDMA1_Channel0);

    if (HAL_DMA_ConfigChannelAttributes(&handle_GPDMA1_Channel0, DMA_CHANNEL_NPRIV) != HAL_OK)
    {
      Error_Handler();
    }

    /* SPI1 interrupt Init */
    HAL_NVIC_SetPriority(SPI1_IRQn, 0, 0);
    HAL_NVIC_EnableIRQ(SPI1_IRQn);
  /* USER CODE BEGIN SPI1_MspInit 1 */

  /* USER CODE END SPI1_MspInit 1 */
  }
  else if(spiHandle->Instance==SPI2)
  {
  /* USER CODE BEGIN SPI2_MspInit 0 */

  /* USER CODE END SPI2_MspInit 0 */

  /** Initializes the peripherals clock
  */
    PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_SPI2;
    PeriphClkInit.Spi2ClockSelection = RCC_SPI2CLKSOURCE_SYSCLK;
    if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
    {
      Error_Handler();
    }

    /* SPI2 clock enable */
    __HAL_RCC_SPI2_CLK_ENABLE();

    __HAL_RCC_GPIOB_CLK_ENABLE();
    /**SPI2 GPIO Configuration
    PB13     ------> SPI2_SCK
    PB14     ------> SPI2_MISO
    PB15     ------> SPI2_MOSI
    */
    GPIO_InitStruct.Pin = SPI_CLK_LTE_Pin|SPI_MISO_LTE_Pin|SPI_MOSI_LTE_Pin;
    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
    GPIO_InitStruct.Alternate = GPIO_AF5_SPI2;
    HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

    /* SPI2 DMA Init */
    /* GPDMA1_REQUEST_SPI2_RX Init */
    handle_GPDMA1_Channel12.Instance = GPDMA1_Channel12;
    handle_GPDMA1_Channel12.Init.Request = GPDMA1_REQUEST_SPI2_RX;
    handle_GPDMA1_Channel12.Init.BlkHWRequest = DMA_BREQ_SINGLE_BURST;
    handle_GPDMA1_Channel12.Init.Direction = DMA_PERIPH_TO_MEMORY;
    handle_GPDMA1_Channel12.Init.SrcInc = DMA_SINC_FIXED;
    handle_GPDMA1_Channel12.Init.DestInc = DMA_DINC_FIXED;
    handle_GPDMA1_Channel12.Init.SrcDataWidth = DMA_SRC_DATAWIDTH_BYTE;
    handle_GPDMA1_Channel12.Init.DestDataWidth = DMA_DEST_DATAWIDTH_BYTE;
    handle_GPDMA1_Channel12.Init.Priority = DMA_LOW_PRIORITY_LOW_WEIGHT;
    handle_GPDMA1_Channel12.Init.SrcBurstLength = 1;
    handle_GPDMA1_Channel12.Init.DestBurstLength = 1;
    handle_GPDMA1_Channel12.Init.TransferAllocatedPort = DMA_SRC_ALLOCATED_PORT0|DMA_DEST_ALLOCATED_PORT0;
    handle_GPDMA1_Channel12.Init.TransferEventMode = DMA_TCEM_BLOCK_TRANSFER;
    handle_GPDMA1_Channel12.Init.Mode = DMA_NORMAL;
    if (HAL_DMA_Init(&handle_GPDMA1_Channel12) != HAL_OK)
    {
      Error_Handler();
    }

    __HAL_LINKDMA(spiHandle, hdmarx, handle_GPDMA1_Channel12);

    if (HAL_DMA_ConfigChannelAttributes(&handle_GPDMA1_Channel12, DMA_CHANNEL_NPRIV) != HAL_OK)
    {
      Error_Handler();
    }

    /* GPDMA1_REQUEST_SPI2_TX Init */
    handle_GPDMA1_Channel11.Instance = GPDMA1_Channel11;
    handle_GPDMA1_Channel11.Init.Request = GPDMA1_REQUEST_SPI2_TX;
    handle_GPDMA1_Channel11.Init.BlkHWRequest = DMA_BREQ_SINGLE_BURST;
    handle_GPDMA1_Channel11.Init.Direction = DMA_PERIPH_TO_MEMORY;
    handle_GPDMA1_Channel11.Init.SrcInc = DMA_SINC_FIXED;
    handle_GPDMA1_Channel11.Init.DestInc = DMA_DINC_FIXED;
    handle_GPDMA1_Channel11.Init.SrcDataWidth = DMA_SRC_DATAWIDTH_BYTE;
    handle_GPDMA1_Channel11.Init.DestDataWidth = DMA_DEST_DATAWIDTH_BYTE;
    handle_GPDMA1_Channel11.Init.Priority = DMA_LOW_PRIORITY_LOW_WEIGHT;
    handle_GPDMA1_Channel11.Init.SrcBurstLength = 1;
    handle_GPDMA1_Channel11.Init.DestBurstLength = 1;
    handle_GPDMA1_Channel11.Init.TransferAllocatedPort = DMA_SRC_ALLOCATED_PORT0|DMA_DEST_ALLOCATED_PORT0;
    handle_GPDMA1_Channel11.Init.TransferEventMode = DMA_TCEM_BLOCK_TRANSFER;
    handle_GPDMA1_Channel11.Init.Mode = DMA_NORMAL;
    if (HAL_DMA_Init(&handle_GPDMA1_Channel11) != HAL_OK)
    {
      Error_Handler();
    }

    __HAL_LINKDMA(spiHandle, hdmatx, handle_GPDMA1_Channel11);

    if (HAL_DMA_ConfigChannelAttributes(&handle_GPDMA1_Channel11, DMA_CHANNEL_NPRIV) != HAL_OK)
    {
      Error_Handler();
    }

    /* SPI2 interrupt Init */
    HAL_NVIC_SetPriority(SPI2_IRQn, 0, 0);
    HAL_NVIC_EnableIRQ(SPI2_IRQn);
  /* USER CODE BEGIN SPI2_MspInit 1 */

  /* USER CODE END SPI2_MspInit 1 */
  }
  else if(spiHandle->Instance==SPI3)
  {
  /* USER CODE BEGIN SPI3_MspInit 0 */

  /* USER CODE END SPI3_MspInit 0 */

  /** Initializes the peripherals clock
  */
    PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_SPI3;
    PeriphClkInit.Spi3ClockSelection = RCC_SPI3CLKSOURCE_HSI;
    if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
    {
      Error_Handler();
    }

    /* SPI3 clock enable */
    __HAL_RCC_SPI3_CLK_ENABLE();

    __HAL_RCC_GPIOD_CLK_ENABLE();
    __HAL_RCC_GPIOG_CLK_ENABLE();
    /**SPI3 GPIO Configuration
    PD6     ------> SPI3_MOSI
    PG9     ------> SPI3_SCK
    PG10     ------> SPI3_MISO
    */
    GPIO_InitStruct.Pin = SPI_MOSI_WIFI_Pin;
    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
    GPIO_InitStruct.Alternate = GPIO_AF5_SPI3;
    HAL_GPIO_Init(SPI_MOSI_WIFI_GPIO_Port, &GPIO_InitStruct);

    GPIO_InitStruct.Pin = SPI_CLK_W_IFI_Pin|SPI_MISO_WIFI_Pin;
    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
    GPIO_InitStruct.Alternate = GPIO_AF6_SPI3;
    HAL_GPIO_Init(GPIOG, &GPIO_InitStruct);

    /* SPI3 DMA Init */
    /* GPDMA1_REQUEST_SPI3_RX Init */
    handle_GPDMA1_Channel10.Instance = GPDMA1_Channel10;
    handle_GPDMA1_Channel10.Init.Request = GPDMA1_REQUEST_SPI3_RX;
    handle_GPDMA1_Channel10.Init.BlkHWRequest = DMA_BREQ_SINGLE_BURST;
    handle_GPDMA1_Channel10.Init.Direction = DMA_PERIPH_TO_MEMORY;
    handle_GPDMA1_Channel10.Init.SrcInc = DMA_SINC_FIXED;
    handle_GPDMA1_Channel10.Init.DestInc = DMA_DINC_FIXED;
    handle_GPDMA1_Channel10.Init.SrcDataWidth = DMA_SRC_DATAWIDTH_BYTE;
    handle_GPDMA1_Channel10.Init.DestDataWidth = DMA_DEST_DATAWIDTH_BYTE;
    handle_GPDMA1_Channel10.Init.Priority = DMA_LOW_PRIORITY_LOW_WEIGHT;
    handle_GPDMA1_Channel10.Init.SrcBurstLength = 1;
    handle_GPDMA1_Channel10.Init.DestBurstLength = 1;
    handle_GPDMA1_Channel10.Init.TransferAllocatedPort = DMA_SRC_ALLOCATED_PORT0|DMA_DEST_ALLOCATED_PORT0;
    handle_GPDMA1_Channel10.Init.TransferEventMode = DMA_TCEM_BLOCK_TRANSFER;
    handle_GPDMA1_Channel10.Init.Mode = DMA_NORMAL;
    if (HAL_DMA_Init(&handle_GPDMA1_Channel10) != HAL_OK)
    {
      Error_Handler();
    }

    __HAL_LINKDMA(spiHandle, hdmarx, handle_GPDMA1_Channel10);

    if (HAL_DMA_ConfigChannelAttributes(&handle_GPDMA1_Channel10, DMA_CHANNEL_NPRIV) != HAL_OK)
    {
      Error_Handler();
    }

    /* GPDMA1_REQUEST_SPI3_TX Init */
    handle_GPDMA1_Channel9.Instance = GPDMA1_Channel9;
    handle_GPDMA1_Channel9.Init.Request = GPDMA1_REQUEST_SPI3_TX;
    handle_GPDMA1_Channel9.Init.BlkHWRequest = DMA_BREQ_SINGLE_BURST;
    handle_GPDMA1_Channel9.Init.Direction = DMA_PERIPH_TO_MEMORY;
    handle_GPDMA1_Channel9.Init.SrcInc = DMA_SINC_FIXED;
    handle_GPDMA1_Channel9.Init.DestInc = DMA_DINC_FIXED;
    handle_GPDMA1_Channel9.Init.SrcDataWidth = DMA_SRC_DATAWIDTH_BYTE;
    handle_GPDMA1_Channel9.Init.DestDataWidth = DMA_DEST_DATAWIDTH_BYTE;
    handle_GPDMA1_Channel9.Init.Priority = DMA_LOW_PRIORITY_LOW_WEIGHT;
    handle_GPDMA1_Channel9.Init.SrcBurstLength = 1;
    handle_GPDMA1_Channel9.Init.DestBurstLength = 1;
    handle_GPDMA1_Channel9.Init.TransferAllocatedPort = DMA_SRC_ALLOCATED_PORT0|DMA_DEST_ALLOCATED_PORT0;
    handle_GPDMA1_Channel9.Init.TransferEventMode = DMA_TCEM_BLOCK_TRANSFER;
    handle_GPDMA1_Channel9.Init.Mode = DMA_NORMAL;
    if (HAL_DMA_Init(&handle_GPDMA1_Channel9) != HAL_OK)
    {
      Error_Handler();
    }

    __HAL_LINKDMA(spiHandle, hdmatx, handle_GPDMA1_Channel9);

    if (HAL_DMA_ConfigChannelAttributes(&handle_GPDMA1_Channel9, DMA_CHANNEL_NPRIV) != HAL_OK)
    {
      Error_Handler();
    }

    /* SPI3 interrupt Init */
    HAL_NVIC_SetPriority(SPI3_IRQn, 0, 0);
    HAL_NVIC_EnableIRQ(SPI3_IRQn);
  /* USER CODE BEGIN SPI3_MspInit 1 */

  /* USER CODE END SPI3_MspInit 1 */
  }
}

void HAL_SPI_MspDeInit(SPI_HandleTypeDef* spiHandle)
{

  if(spiHandle->Instance==SPI1)
  {
  /* USER CODE BEGIN SPI1_MspDeInit 0 */

  /* USER CODE END SPI1_MspDeInit 0 */
    /* Peripheral clock disable */
    __HAL_RCC_SPI1_CLK_DISABLE();

    /**SPI1 GPIO Configuration
    PG2     ------> SPI1_SCK
    PG3     ------> SPI1_MISO
    PG4     ------> SPI1_MOSI
    */
    HAL_GPIO_DeInit(GPIOG, FL1_SCK_Pin|FL1_SO_Pin|FL1_SI_Pin);

    /* SPI1 DMA DeInit */
    HAL_DMA_DeInit(spiHandle->hdmarx);
    HAL_DMA_DeInit(spiHandle->hdmatx);

    /* SPI1 interrupt Deinit */
    HAL_NVIC_DisableIRQ(SPI1_IRQn);
  /* USER CODE BEGIN SPI1_MspDeInit 1 */

  /* USER CODE END SPI1_MspDeInit 1 */
  }
  else if(spiHandle->Instance==SPI2)
  {
  /* USER CODE BEGIN SPI2_MspDeInit 0 */

  /* USER CODE END SPI2_MspDeInit 0 */
    /* Peripheral clock disable */
    __HAL_RCC_SPI2_CLK_DISABLE();

    /**SPI2 GPIO Configuration
    PB13     ------> SPI2_SCK
    PB14     ------> SPI2_MISO
    PB15     ------> SPI2_MOSI
    */
    HAL_GPIO_DeInit(GPIOB, SPI_CLK_LTE_Pin|SPI_MISO_LTE_Pin|SPI_MOSI_LTE_Pin);

    /* SPI2 DMA DeInit */
    HAL_DMA_DeInit(spiHandle->hdmarx);
    HAL_DMA_DeInit(spiHandle->hdmatx);

    /* SPI2 interrupt Deinit */
    HAL_NVIC_DisableIRQ(SPI2_IRQn);
  /* USER CODE BEGIN SPI2_MspDeInit 1 */

  /* USER CODE END SPI2_MspDeInit 1 */
  }
  else if(spiHandle->Instance==SPI3)
  {
  /* USER CODE BEGIN SPI3_MspDeInit 0 */

  /* USER CODE END SPI3_MspDeInit 0 */
    /* Peripheral clock disable */
    __HAL_RCC_SPI3_CLK_DISABLE();

    /**SPI3 GPIO Configuration
    PD6     ------> SPI3_MOSI
    PG9     ------> SPI3_SCK
    PG10     ------> SPI3_MISO
    */
    HAL_GPIO_DeInit(SPI_MOSI_WIFI_GPIO_Port, SPI_MOSI_WIFI_Pin);

    HAL_GPIO_DeInit(GPIOG, SPI_CLK_W_IFI_Pin|SPI_MISO_WIFI_Pin);

    /* SPI3 DMA DeInit */
    HAL_DMA_DeInit(spiHandle->hdmarx);
    HAL_DMA_DeInit(spiHandle->hdmatx);

    /* SPI3 interrupt Deinit */
    HAL_NVIC_DisableIRQ(SPI3_IRQn);
  /* USER CODE BEGIN SPI3_MspDeInit 1 */

  /* USER CODE END SPI3_MspDeInit 1 */
  }
}

the same application works well with the STM32H723 micro but we needed more RAM

 

1 REPLY 1
Saket_Om
ST Employee

Hello @franckngatcha 

When using DMA on microcontrollers with data cache, such as the STM32U5 series, it is essential to manage cache coherency to ensure data integrity between the CPU and DMA. Before starting a DMA receive operation, you should clean the data cache for the target buffer using SCB_CleanDCache_by_Addr((uint32_t*)buffer, size); to ensure that any modified data in the cache is written back to RAM, making the buffer ready for DMA access. After the DMA transfer is complete, you must invalidate the cache for the same buffer with SCB_InvalidateDCache_by_Addr((uint32_t*)buffer, size); so that the CPU fetches the latest data from RAM, reflecting the changes made by the DMA.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Saket_Om