cancel
Showing results for 
Search instead for 
Did you mean: 

STM32U585 - Enhanced secure key storage example code

Surya S
Associate II

Hello all,

Can anyone provide example code - Enhanced secure key storage using stm32u585?

 

Thanks in Advance,

Surya S

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
STea
ST Employee

Hello @Surya S and welcome to ST Community,

You can find example code on the Enhanced secure key storage using stm32u585 in the STM32CUBEH5 STM32Cube_FW_U5_V1.3.0\Projects\B-U585I-IOT02A\Examples\CRYP

you can check the CRYP_SAES_SharedKey project which provides an example of using the Secure AES co-processor (SAES) peripheral to share application keys with AES peripheral.

and the CRYP_SAES_WrapKey project which provides an example of using the Secure AES co-processor (SAES) peripheral to wrap application keys using hardware secret key DHUK then use it to encrypt in polling mode.

this examples could also be obtained from Github .

Hope this answers your request .

BR

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
STea
ST Employee

Hello @Surya S and welcome to ST Community,

You can find example code on the Enhanced secure key storage using stm32u585 in the STM32CUBEH5 STM32Cube_FW_U5_V1.3.0\Projects\B-U585I-IOT02A\Examples\CRYP

you can check the CRYP_SAES_SharedKey project which provides an example of using the Secure AES co-processor (SAES) peripheral to share application keys with AES peripheral.

and the CRYP_SAES_WrapKey project which provides an example of using the Secure AES co-processor (SAES) peripheral to wrap application keys using hardware secret key DHUK then use it to encrypt in polling mode.

this examples could also be obtained from Github .

Hope this answers your request .

BR

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.