Skip to main content
Associate
September 1, 2025
Solved

STM32N6 CMSIS-DSP arm_rfft_q31 hard fault with M55 MVE, runs with ARM_MATH_AUTOVECTORIZE

  • September 1, 2025
  • 1 reply
  • 526 views

Has anyone had success with the CMSIS-DSP arm_rfft_q31 or other of the M55 HELIUM MVEI/MVEF enabled CMSIS-DSP functions on the STM32N6? 

Is there a functional FFT example or STM32CubeMX project available? The STM32N6 FE 1.2.0 example CORTEX-HELIUM does not seem to utilize CMSIS-DSP.

Whenever I try to utilize the CMSIS-DSP FFT-functions, I am experiencing hard fault when entering the arm_rfft_q31, function, if the M55 HELIUM MVEI/MVEF support is enabled.

My FSBL project builds successfully and I am currently using ARM_MATH_AUTOVECTORIZE as a temporary solution, with limited performance.

Please let me know for working examples, tips, or known caveats of using CMSIS-DSP with HELIUM MVEI/MVEF on STM32N6. I am looking for proof, that the STM32N6 MVEI and MVEF are functional and supported with CMSIS-DSP.

Thanks!

 

Best answer by Saket_Om

Hello @jylho 

Unfortunately, ST does not provide examples on FFT.

1 reply

ST Technical Moderator
September 2, 2025
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
jylhoAuthor
Associate
September 2, 2025

Thanks @Saket_Om for your fast response.

I have success on using CMSIS-DSP according to the ARM provided examples, but only if the build target is cortex-m33 or by using the ARM_MATH_AUTOVECTORIZE.

The build target cortex-m55 without ARM_MATH_AUTOVECTORIZE doesn't seem to work, causing a hard fault.

It might relate to the data alignment. I will further debug the hard fault according to the knowledge base, but seems the article does not cover the STM32N6 related details like AFSR, got some details for further debugging from https://community.st.com/t5/stm32-mcus-products/stm32n6-hard-fault-when-accessing-tcm/td-p/757557

It seems I am missing some STM32N6 specific configuration in STM32CubeMX, so I would really appreciate an example of FFT utilizing M55 HELIUM, provided or supported by ST, to see that the ST provided toolchain works with MVEI and MVEF on the STM32N6.

An example project for NUCLEO or DK board would be ok, as I have both.

Thanks!

Saket_OmBest answer
ST Technical Moderator
September 5, 2025

Hello @jylho 

Unfortunately, ST does not provide examples on FFT.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om