2022-04-11 4:45 PM
Hi,
I'm using SAI in I2S mode to play stereo wav file. Audio Data is sent to TAS5722l which is a Mono Audio amplifier. My problem is that the FS (Frame Synchronization) signal
stays always at level High. This results in a stereo audio file being played in twice its original duration as each samples from both channels are read by the amplifier.
Bellow is SAI initialilzation generated by CubeMx:
hsai_BlockA1.Instance = SAI1_Block_A;
hsai_BlockA1.Init.AudioMode = SAI_MODEMASTER_TX;
hsai_BlockA1.Init.Synchro = SAI_ASYNCHRONOUS;
hsai_BlockA1.Init.OutputDrive = SAI_OUTPUTDRIVE_DISABLE;
hsai_BlockA1.Init.NoDivider = SAI_MASTERDIVIDER_ENABLE;
hsai_BlockA1.Init.FIFOThreshold = SAI_FIFOTHRESHOLD_EMPTY;
hsai_BlockA1.Init.AudioFrequency = SAI_AUDIO_FREQUENCY_48K;
hsai_BlockA1.Init.SynchroExt = SAI_SYNCEXT_DISABLE;
hsai_BlockA1.Init.MonoStereoMode = SAI_STEREOMODE;
hsai_BlockA1.Init.CompandingMode = SAI_NOCOMPANDING;
hsai_BlockA1.Init.TriState = SAI_OUTPUT_NOTRELEASED;
if (HAL_SAI_InitProtocol(&hsai_BlockA1, SAI_I2S_STANDARD, SAI_PROTOCOL_DATASIZE_32BIT, 2) != HAL_OK)
{
Error_Handler();
}
Thanks in advance for your help
2022-07-05 11:16 PM
Hi, did you already solve your problem? I have a similar problem like you, I have my stereo wav file and I wanna play it on a stereo audio amplifier, but how can I control the WS(Word Select, left/right channel select) pin? Does WS pin automatically switch between 0 and 1 when every frame is sent?