2015-06-23 1:16 AM
I made my own bootloader for an STM32L1 board. My algorithm is simple : - first, I erase the memory I need to write my new program on my flash. - then, I write 4 bytes per 4 bytes my new program ( I receive it from the USART of the board)
My new program should blink a LED but nothing happens and I d'ont understand why ...
Do i have to write my own RESET function? Here is my code if you want to give a try.
void BootLoader(void) {
//clear all ITs
USART_ITConfig_boot( USART1, USART_IT_RXNE, 0);
uint32_t start_adr, end_adr;
uint8_t status, i;
uint8_t buffer[4096];
uint8_t sizeRcv[2];
uint16_t tailleSector = 0x1000;
uint32_t adr;
uint8_t nbSector = 0;
//size fixée en dur
uint16_t k = 0;
uint8_t size1 = 0;
uint8_t size2 = 0;
uint16_t sizeBin = 0;
//taille sector
uint16_t tailleSecteurDec = 4096;
SendString_boot(''BOOTLOADER ON.....\r\n'', USART2);
//adress
//First Sector
start_adr = WRITE_START_ADDR;
end_adr = start_adr + tailleSector;
//erasing flags
FLASH_ClearFlag_boot(
FLASH_FLAG_EOP | FLASH_FLAG_WRPERR | FLASH_FLAG_PGAERR
| FLASH_FLAG_SIZERR | FLASH_FLAG_OPTVERR
| FLASH_FLAG_OPTVERRUSR | FLASH_FLAG_RDERR);
FLASH_Unlock_boot();
sizeBin = 51400;
nbSector = (uint8_t) (sizeBin / tailleSecteurDec) + 1;
if(nbSector > 30){
SendString_boot(''cannot overrite memory : too much sectors used\r\n'',USART2);
}
for (i = 0; i <= (127 - 1); i++) {
if(end_adr <
0x0808FFFF
){
status
=
Flash_Erase
(start_adr, end_adr);
start_adr
=
end_adr
;
end_adr
= end_adr + tailleSector;
SendString_boot('' ERASING SECTOR DONE \r\n'', USART2);
}
else{
SendString_boot(''END OF FLASH MEMORY\r\n'', USART2);
}
}
SendString_boot(''ERASING COMPLETE\r\n'', USART2);
start_adr
=
WRITE_START_ADDR
;
//receive frames
adr
=
WRITE_START_ADDR
;
do {
SendString_boot(''ACK_READY'', USART1);
SendString_boot(''ACK_READY\r\n'', USART2);
//receive 32 bytes
if (sizeBin - k > 4096)
Receive_Data_boot(buffer, 4096);
else
Receive_Data_boot(buffer, sizeBin - k);
//write 32 bytes in memory
if (sizeBin - k > 4096)
status = Flash_Write(adr, buffer, 4096);
else
status = Flash_Write(adr, buffer, sizeBin - k);
//on check si on ecrit bien au bon endroit
//increment cpt
k = k + 4096;
adr = adr + 0x1000;
i++;
//check CRC
//TODO
SendString_boot(''...FLASH DONE ON '', USART2);
SendString_boot(''\r\n'', USART2);
SendString_boot('' SECTOR DONE \r\n'', USART2);
} while (k < sizeBin);
SendString_boot(''END'', USART1);
SendString_boot(''ACK_END\r\n'', USART2);
FLASH_Lock_boot();
}
#stm32 #bootloader #c
2015-06-23 3:54 AM
Ok, and where exactly does it write this image, and transfer control to it?
Perhaps you can debug by sending progress data via the USART, and confirm your uploaded image is valid.The easiest way of doing this is to have the uploaded image use it's own vector table, and reset handler entry point.Review the available IAP examples for this and other STM32 families.