2017-02-10 11:30 AM
Datasheet does not explain the settings corresponding to boot0 pin high or low - could I please get some information on this for the csp-49 package which only has boot0 and no other boot configuration pins.
#stm32l #boot #stm322017-02-10 12:38 PM
The Reference Manual?
2017-02-10 4:10 PM
Yeah still useless, it has settings with a boot0 and boot1 pin. The stm32l082cz only has boot0
2017-02-10 5:42 PM
Boot1 is stored in the option bytes. For most purposes Boot0 switches between ROM and FLASH. As defined in the RM.