cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H750IB getting into persistent problem with SCB_EnableDCache

TallMike
Associate III

Hi, We've been using a board (the Daisy Seed) that has an STM32H750IB and external QSPI flash chip.

We're having an issue with some of the boards somehow getting into a persistent (across reset. power cycle, and chip erase) state whereby the SCB_EnableDCache function is taking several seconds to execute.  Even stranger, when DCaching is disabled, then the QSPI init call takes several seconds.   Most of the boards are working fine, but somehow something happens and the board/chip will start doing this.  In one case, it just as randomly stopped doing it. 

    Could some kind of un-initialized variable be causing this?

     Also, we're using an older version of CMSIS code (Ver 5.0.1), has anything been fixed or changed in the newer versions?

 

23 REPLIES 23

My primary concern would be with the VCAP capacitors, either one 4u7 or a pair or 2u2

Inadequate, low ESR, capacitance here is the source of a lot of quirky behaviour

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Here's a picture.

stm_cpu.JPEG

Looks like it's 2 of the 2.2 uF caps, one on each VCAP pin.  Don't have the part number, however.

The QSPI is not being used in Memory-mapped / XIP mode, just as external storage, so do we still need to set up the 0x90000000 region?

 

TallMike
Associate III

Update: Interesting and unsettling new data point:
I plugged and unplugged the Daisy Seed board (stand-alone, using the on-board USB port) about 20 times, and it suddenly started behaving again!

What you think...? 

AScha3_0-1720247968023.png

 

If you feel a post has answered your question, please click "Accept as Solution".

Looks like a 'V'

But still having this super weird seemingly impossible unexplainable inexplicable situation!

Any ideas?

How is it even possible?

 

Hi, just wanted to follow up and see if there's any progress on figuring this out?  It's got us quite worried about shipping a board until this is resolved.

 

I don't think anyone here has advanced your issue, you should perhaps escalate with Electro-Smith, or your local ST Micro FAE if you're working with them. Did you get a better schematic from them?

You could open your own support ticket via the online support system https://ols.st.com/s/

Can't say I've seen any other Daisy Board users here.

Odd behaviour tends to be power related, or with Internal Flash timing. If clocks don't start things can be relatively slow. The H7 starts on a 64MHz HSI, you can continue to use that without doing anything, and output via a serial port to understand internal state and progress.

Should see 1.25 V on the + side of the VCAP's, you could perhaps look at supply stability there, and the 3.3V rails.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..