cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H747I with LWIP not working

YZhen.4
Associate II

Hello

I used the STM32H747-Disco development board and created a Keil project according to this link, https://community.st.com/s/article/How-to-create-project-for-STM32H7-with-Ethernet-and-LwIP -stack-working

My CubeMX is version 6.6, and the firmware package is version 1.10, but my Lwip can't work properly. During the debugging process, I found that there is a problem with the initialization part of Lan8742, and it returns a timeout problem LAN8742_STATUS_RESET_TIMEOUT

The problem is here lan8742.c :

      while(regvalue & LAN8742_BCR_SOFT_RESET)

      {

       if((pObj->IO.GetTick() - tickstart) <= LAN8742_SW_RESET_TO)

       {

        if(pObj->IO.ReadReg(pObj->DevAddr, LAN8742_BCR, &regvalue) < 0)

        { 

         status = LAN8742_STATUS_READ_ERROR;

         break;

        }

       }

       else

       {

        status = LAN8742_STATUS_RESET_TIMEOUT;

        break;

       }

      } 

Can someone help me please:loudly_crying_face:

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4

The first thing to do would be to observe signal on MDIO/MCLK to find out whether the SMI interface works.

If not, the most common problem at this stage is missing or misconfigured ETH module clock, so check if it's physically present on the required pin, that that pin is properly configured in GPIO and that any enable/steering bits are set properly. I don't use the 'H747 so don't know what the relevant details may be.

JW

[EDIT] ... and don't forget to check any related jumpers/solder bridges on the Disco board, too...

YZhen.4
Associate II

Hello

How to observe the signals on MDIO/MCLK to determine whether the SMI interface works.

The official disco development board I used should be free of hardware problems, and my IO configuration is as follows, which is also consistent with the official schematic diagram.

void HAL_ETH_MspInit(ETH_HandleTypeDef* ethHandle)

{

 GPIO_InitTypeDef GPIO_InitStruct = {0};

 if(ethHandle->Instance==ETH)

 {

 /* USER CODE BEGIN ETH_MspInit 0 */

 /* USER CODE END ETH_MspInit 0 */

  /* Enable Peripheral clock */

  __HAL_RCC_ETH1MAC_CLK_ENABLE();

  __HAL_RCC_ETH1TX_CLK_ENABLE();

  __HAL_RCC_ETH1RX_CLK_ENABLE();

  __HAL_RCC_GPIOG_CLK_ENABLE();

  __HAL_RCC_GPIOC_CLK_ENABLE();

  __HAL_RCC_GPIOA_CLK_ENABLE();

  /**ETH GPIO Configuration

  PG11   ------> ETH_TX_EN

  PG12   ------> ETH_TXD1

  PG13   ------> ETH_TXD0

  PC1   ------> ETH_MDC

  PA2   ------> ETH_MDIO

  PA1   ------> ETH_REF_CLK

  PA7   ------> ETH_CRS_DV

  PC4   ------> ETH_RXD0

  PC5   ------> ETH_RXD1

  */

  GPIO_InitStruct.Pin = ETH_TX_EN_Pin|ETH_TXD1_Pin|ETH_TXD0_Pin;

  GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

  GPIO_InitStruct.Pull = GPIO_NOPULL;

  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;

  GPIO_InitStruct.Alternate = GPIO_AF11_ETH;

  HAL_GPIO_Init(GPIOG, &GPIO_InitStruct);

  GPIO_InitStruct.Pin = ETH_MDC_SAI4_D1_Pin|ETH_RXD0_Pin|ETH_RXD1_Pin;

  GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

  GPIO_InitStruct.Pull = GPIO_NOPULL;

  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;

  GPIO_InitStruct.Alternate = GPIO_AF11_ETH;

  HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

  GPIO_InitStruct.Pin = ETH_MDIO_Pin|ETH_REF_CLK_Pin|ETH_CRS_DV_Pin;

  GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

  GPIO_InitStruct.Pull = GPIO_NOPULL;

  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;

  GPIO_InitStruct.Alternate = GPIO_AF11_ETH;

  HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

  /* Peripheral interrupt init */

  HAL_NVIC_SetPriority(ETH_IRQn, 5, 0);

  HAL_NVIC_EnableIRQ(ETH_IRQn);

 /* USER CODE BEGIN ETH_MspInit 1 */

 /* USER CODE END ETH_MspInit 1 */

 }

}

> How to observe the signals on MDIO/MCLK to determine whether the SMI interface works.

Using oscilloscope/logic analyzer.

Also, using oscilloscope/logic analyzer check presence of clock at the PA1=ETH_REF_CLK pin.

Also check in RM (Reference Manual), which register bits (RCC, SYSCFG) have to be set for ETH to operate properly.

> The official disco development board I used should be free of hardware problems,

It probably is, but you may need to set jumpers/solder bridges properly, and you may need to switch on features in software. I don't use the 'H7 nor this Disco board, so don't know the details; have a look at the schematics and at the Disco board's User Manual.

JW

YZhen.4
Associate II

Thank you very much for your guidance. I will try