2019-06-25 5:26 AM
I am sorry that I am not good at English.
Hi.
I use the stm32h743zi mcu.
I ported stm32h743i-val lwip tcp echo server and client application
server application was well working but client was not working
ping test was not responed.
my firmware flow is this
lwip init -> tcp_echoclient init -> lwip process
i don't use RTOS
2020-08-05 4:37 AM
Hi Piranha,
thank You for the answer.
I am trying to implemented recommended changes, but I am not able to do them all. I am using stm32f417 chip. I am generating cubeMX project with RTOS and LWIP with firmware package STM32Cube_FW_F4_V1.25.0 and cubeMX version 5.6.1
from the list You provided:
I have added these modifications:
1.
i added ad the end of function MX_LWIP_Init() in the lwip.c:
ETH->MACIMR = ETH_MACIMR_TSTIM | ETH_MACIMR_PMTIM;
ETH->MMCRIMR = ETH_MMCRIMR_RGUFM | ETH_MMCRIMR_RFAEM | ETH_MMCRIMR_RFCEM;
ETH->MMCTIMR = ETH_MMCTIMR_TGFM | ETH_MMCTIMR_TGFMSCM | ETH_MMCTIMR_TGFSCM;
2.
I added function MPU_Config() and call it at the end of main function inicialization.
void MPU_Config(void)
{
MPU_Region_InitTypeDef MPU_InitStruct;
/* Disables the MPU */
HAL_MPU_Disable();
/**Initializes and configures the Region and the memory to be protected
*/
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER2;
...
The rest I am not able to identify what exactly should i change and where.
1.
from the point:
https://community.st.com/s/question/0D50X0000C4Nk4GSQS/bug-missing-compiler-and-cpu-memory-barriers
I cannot locate OWN bit so i do not know where to add __DMB()
2.
this is very confusion, no clue what should be done.
3.
this one is last one applicable for stm32f4
lwIP API related:
I use fixed IP address, so no DHCP is used.
anybody could help please?
Thank You.
Peter
2020-08-06 12:50 AM
Could enyone help please? I really cannot move from this place.
Thank You.
Peter
2020-08-07 5:58 AM
Hi ST comunity, could somebody please provide CubeMX file with RTOS and LWIP properly setup for stm32f4* chip ,that will generate project, which i could use for running TCP client?
Thank You.
Peter
2020-08-09 6:14 AM
ST Community,
I am stuck at TCP client for STM32f4. Could anybody please give me working example for the STM32f4 chip family?
Thanks a lot!
Peter
2020-08-10 1:00 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.