2023-09-13 3:34 AM
2023-09-13 6:31 AM
What do you mean by switching? Do you want only one function at any time, or both simultaneously (a composite device)?
2023-09-13 6:37 AM
dual/composite device : just an example ->
>> This application provides an example of Azure RTOS USBX stack usage on STM32H747I-DISCO board, it shows how to develop a composite USB Device communication Class "HID" and "CDC_ACM" based application.
2023-09-13 11:36 PM
By switching i mean, only one function at any time. The DFU Upload mode then should be started by a defined CDC command.
2023-09-18 6:50 AM
Thanks for the example, but how can i migrate such a project to my hardware? I tried by creating and comparing and merging a new project for my hardware but without any success. Do you have any tip?
2023-09-21 6:09 AM
I now was able to create a project including CDC_ACM and DFU and the initialization also looks well. The code is similar to the other example with CDC_ACM and HID.
Nevertheless i have problems to run it at the target device STM32H735. In the debug session that function call _tx_thread_schedule(); never returns.
Does anyone have any idea, what I'm doing wrong?
Attached I have the project.
Thanks in advance.