cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 - 1 port and 2 interfaces

inigo1
Associate II

Hello,

I am designing a device and one of the requirements is that two interfaces can be managed with the same ethernet port. One interface must be fully configurable (IP, mask and gateway) and the other can only be accessed locally (fixed IP and mask).

I am using a NUCLEO-H723ZG that has a LAN8742A Ic and I would like to know if it is possible to do it.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0