cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G4 trigger SPI-DMA transfer with timer

Smallface
Associate II

Hello,

I want to trigger a SPI-transfer with a timer. Its like in this post:

https://community.st.com/t5/stm32-mcus-embedded-software/stm32g4-trigger-dma-request-from-spi-to-memory-with-timer/td-p/726370

but I want that an output compare of a timer that triggers an SPI-DMA transfer. The SPI in the STM should run as a slave.

An external ADC is always triggererd from an other timer an sends his data on the SPI as a master. The SPI in the STM should read 1034x16bit values in an buffer.

I began to try it with CUBE-IDE and HAL functions. Than I found this thread here and wrote it for my application (see code below) but also with these functions i could not start the SPI-DMA transfer.

 

Is it not possible to start a spi-dma-slave for 1034 values?

Many thanks.

 

 

 

uint16_t circular_buffer[1034]; void acq_configure_adc_transfer() { // Read SPI1 data after rx to buffer DMA1_Channel2->CCR = 0x0; //Disable DMA stream DMA1_Channel2->CPAR = (uint32_t)&SPI1->DR; //Set peripheral data register as destination DMA1_Channel2->CMAR = (uint32_t)&circular_buffer; //Set source memory region DMA1_Channel2->CNDTR = sizeof(circular_buffer) ; //Number of items to transfer DMA1_Channel2->CCR =DMA_CCR_EN | //Enable DMA_CCR_HTIE | //half transfer interrupt enable DMA_CCR_TCIE | //transfer complete interrupt enable DMA_CCR_CIRC | //DMA Circular mode DMA_PINC_DISABLE | //Do not increment peripheral DMA_MINC_ENABLE | //Do increment memory DMA_CCR_PSIZE_0 | //Peripheral data size 0 = 16bit , 1 = 32bit DMA_CCR_MSIZE_0 | //Memory data size 0 = 16bit , 1 = 32bit DMA_PRIORITY_VERY_HIGH; //DMA Priority DMAMUX1_Channel0->CCR = 0; DMAMUX1_Channel0->CCR |= DMA_REQUEST_TIM1_UP | DMAMUX_CxCR_EGE; DMAMUX1_Channel1->CCR = 0; DMAMUX1_Channel1->CCR |= DMA_REQUEST_SPI1_RX | DMAMUX_CxCR_EGE; HAL_TIM_Base_Start(&htim1); //Start Timer //Reset SPI1 Configuration Register SPI1->CR1 = 0; SPI1->CR2 = SPI_CR2_RXDMAEN | SPI_CR2_TXDMAEN | SPI_CR2_NSSP | SPI_CR2_SSOE | SPI_DATASIZE_16BIT; // TXDMAEN: Enable TX dma, SSOE:SSoutputenable, , Data frame format 16bit SPI1->CR1 = SPI_CR1_SPE; //Enable SPI, configuration as slaver //Reset Timer Configuration Registers TIM1->CR1 = 0; TIM1->CR2 = 0; TIM1->DIER = TIM_DIER_UDE; //UDE Update DMA request enable TIM1->PSC = 500; //Set the prescaler TIM1->ARR = 1000; //Set the autoreload value (timer interval) TIM1->CR1 = TIM_CR1_CEN | TIM_CR1_ARPE; //the CEN is set (Counter enable) and ARPE:Auto-reloadpreloadenable is buffered (TIMx_ARR register is buffered) //Timer is now started and triggers SPI at each overflow }
View more

 

 

 

3 REPLIES 3
TDK
Super User

A transfer of 1034 elements is possible. The code configures 2068 transfers, not 1034. sizeof(x) returns the size of x in bytes, not the number of elements.

You don't configure the DMA to send to SPI->DR in response to a trigger anywhere. DMA1_Channel1 is not configured.

If you feel a post has answered your question, please click "Accept as Solution".
Smallface
Associate II

Hello TDK,

Thank you for your help.

I can try your corrections first in the next year, I will try it first with a timer overrun like in the sample code

But

I thought in case I configurate the SPI as a slave I dont need the DMA1_Channel1, because I just recieve data.

Perhaps I dont need to set: SPI_CR2_TXDMAEN

 

I also need the HAL_SPI_RxCpltCallback function that after a transfer i can copy the recieved data to another memory.

Which bit must I set so after a transfer the code goes to HAL_SPI_RxCpltCallback.

 

I tried it also to start the SPI DMA read with the cubeMX:

The trigger was here Interrupt from the Input EXTI0, even here it does not worked.

I init it in the main-function with:

#define SIZE_SPI_ADS8509 1036 uint16_t aRxBuffer_SPI_ADS8509[SIZE_SPI_ADS8509]; ret = HAL_SPI_Receive_DMA(&hspi2, (uint8_t *)aRxBuffer_SPI_ADS8509, SIZE_SPI_ADS8509);

Smallface_1-1734619166010.pngSmallface_2-1734619184589.png

 

 

TDK
Super User

Ahh, it's a slave. I missed that. If you're just receiving, then you don't need to worry about TX at all.

In that case, I don't understand what TIM1 is doing here. If you want to receive SPI data into a circular buffer, that can be done without a timer.

If your register level code isn't working, I would suggest coding it up using CubeMX and HAL and HAL_SPI_TransmitReceive_DMA(...), and then copying those register settings. It should be straightforward

If you feel a post has answered your question, please click "Accept as Solution".