Skip to main content
Baris
Visitor II
November 20, 2020
Question

STM32F769i-DISCO Ethernet Speed

  • November 20, 2020
  • 0 replies
  • 439 views

Hello,

I am using STM32F769i-DISCO board in my project. The project include camera module and I get data from this module using DCMI. I want to send this data to computer via ethernet. For this I need at least 100Mbits/s ethernet speed. But I cant find ethernet speeds of this board. I only found following lines in boards manual. And this lines include only "10/100 Mbits" statements. I cant understand actual speed of this board.

Ethernet

The 32F769IDISCOVERY Discovery board supports 10/100-Mbit Ethernet communication

by a PHY LAN8742A-CZ-TR from MICROCHIP and integrated a RJ45 connector. Ethernet

PHY is connected to the STM32F769NIH6 via an RMII interface.

The oscillator X2 generates a 25 MHz clock for the PHY, the PHY RMII_REF_CLK

generates the 50 MHz clock for the STM32F769NIH6.

What is actual speed ethernet in this board?

Can I use this board for my project?

This topic has been closed for replies.