2019-09-25 05:01 AM
Hi,
I try to get the Device-MSC_Standalone run.
It should be play, out of the box.
When I plug the USB-Connector (CN15) to the PC,
an error occur.
Windows-Dev-Maanager stated:
"Error while request Device-Descrpitor"
What is wrong?
Compiler-Option "USE_USB_HS" is never used in the Code.
The Example is based on "STM32Cube_FW_F7_V1.15.0".
see readme.txt
This application has been tested with STMicroelectronics STM32F769I-Discovery...
In the Example-Dir of STM32Cube_FW_L4_V1.14.0.../32L496GDISCOVERY
there is no "MSC-Standalone" at all.
Why not?
Kind Regards
Thomas
2019-10-07 12:15 AM
OK, no answers but new informations...
when connected to PC with OS Windows 7 a STM-Drive appears
and is read-/writeable. (disk.sys/partmgr.sys will be used)
when connected to PC with OS Windows 10,
no driver will be found :(
Is this a common Windows Problem?
Any Recommendation which Driver should be used?
Kind regards
Thomas