2025-12-10 3:51 AM - edited 2025-12-10 4:21 AM
Hi ST Team,
I need to implement USB Host Printer support on STM32F767 using USBX.
I'm trying to send PCL6 (HP LaserJet) print jobs via USB.
Challenge: No Host Printer example exists in stm32-usbx-examples
(only Device Printer and Host MSC/CDC).
What I need:
1. Is USBX Host Printer class available? Any code?
2. How to send binary PCL6 data to printer (USB Bulk OUT)?
3. CubeMX configuration for USB Host (FS/HS)?
4. Printer enumeration and status read examples?
5. Any complete working reference project?
Current Setup:
- STM32F767ZI + FreeRTOS + USBX
- HP LaserJet printer (USB)
- Using HP's jetlib for PCL6 generation
Please advise or point to relevant docs/code.
Thanks,
Madhu07
2025-12-10 6:38 AM
hello @MADHU2
Well USBX host printer class is available. However, So far, no example is provided to cover Printer class as far as I know. CubeMX imports Middleware files and leaves it to developer to tailor their application in app_usbx_host.c/h.
you can check USBX middleware
here is some threads that can help you thread1 thread2 thread3
for cubeMX configuration just ensure that you are sending a clean 48mhz to the USB and you are using the correct pins you can check your product datasheet. You can also review AN4879
Hope that helps for now, I will come back to you if I find any other information
Gyessine
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.