cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F429I-Discovery BSP does not include LED5 & 6?

victagayun
Senior III
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Peter BENSCH
ST Employee

Hi Victor,

What should that make sense for?

LD5/LD6 can only be influenced indirectly by the STM32F429, indicating VBUS and overcurrent at the OTG port.

Best regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
victagayun
Senior III

Hi Peter,

For other purposes not using VBUS and OTG.

---Victor

victagayun
Senior III

Oh, we cannot use the VBUS that is output of STMPS2141STR.

But the /Fault is open drain though.

Peter BENSCH
ST Employee

Well, you could expand the BSP yourself, if you really want to drive LD6. But you have to keep in mind that it is being driven with some kind of wired-or with the STMPS2141, so the status of LD6 depends on OTG_FS_OC and the /FAULT signal from the STMPS2141.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.