2013-10-09 6:35 AM
Hello :)
I just remove the LCD from one of my board and made a R2R Resistor DAC connected to the LCD dedicated pin. The only pins you need are the 3 x 6bits colors , the vsync , hsync and GND. After some changes in one of the examples source from ST i was able to get a picture to my VGA Monitor ;) I just don't have the correct timing for view 640 x 480 picture , the monitor report me a 800 x 600 resolution with 31.4Khz Horizontal and 52.3Hz refresh time ... Hmmm I probably don't understand correctly the data-sheet/app note about the timing. Or i put wrong parameter for sync time + bach porch etc ... For those who want try i attach the source to put in the \Projects\Peripheral_Examples\ directory and the R2R Schematic i do for this test. If someone get the correct timing setup for 640 x 480 resolution i will be happy to get it ;) It's allot more comfortable to play with a big monitor , just no touch screen here , next step is to use a USB KB + Mouse ... he he he Cheers. PS : i compiled this with Keil.. #stm32f429-disco-vga-monitor #32f429-disco-vga-monitor-image #vga-disco-take-it #instead-of-desoldering-the-lcd2013-10-09 8:04 AM
Little update.
I corrected some of my mistake , now i get picture perfect fitted into the screen. made change in :void LCD_Init(void)
{
.....
/* Timing configuration */
/* Configure horizontal synchronization width */
LTDC_InitStruct.LTDC_HorizontalSync = 96;//96
/* Configure vertical synchronization height */
LTDC_InitStruct.LTDC_VerticalSync = 2;//2
/* Configure accumulated horizontal back porch */
LTDC_InitStruct.LTDC_AccumulatedHBP = 144; //HSync + HBP = 144
/* Configure accumulated vertical back porch */
LTDC_InitStruct.LTDC_AccumulatedVBP = 35; //VSync + VBP = 35
/* Configure accumulated active width */
LTDC_InitStruct.LTDC_AccumulatedActiveW = 784;//144 + 640 = 784
/* Configure accumulated active height */
LTDC_InitStruct.LTDC_AccumulatedActiveH = 515;//35 + 480 = 515
/* Configure total width */
LTDC_InitStruct.LTDC_TotalWidth = 800;
/* Configure total height */
LTDC_InitStruct.LTDC_TotalHeigh = 525;
LTDC_Init(<DC_InitStruct);
}
Now i have to found why i don't get uniform colors , in the picture attached you will see that the 'Green' background is changing Anyway , it's a good start :) Cheers.
________________
Attachments : 32f429_capture.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzhX&d=%2Fa%2F0X0000000bPU%2F5EeQ5o6RvWDq3k2cLTpipeWLHD0A_TTT5m75NtnjMmc&asPdf=false
2013-10-09 12:24 PM
I finally found why the colors was not uniform.
we use 18bits / pixels but when we do the SDRAM test , every bits are write and for some reason when we write to Video memory after this we have a 'mix' ;) The easy way to prevent it is to erase the part of the SDRAM we use for the Video. For made simple i just erase all SDRAM after the SDRAM test , it's just a copy/paste from this code :/* Erase SDRAM memory */
for (counter = 0x00; counter < IS42S16400J_SIZE; counter++)
{
*(__IO uint16_t*) (SDRAM_BANK_ADDR + 2*counter) = (uint16_t)0x00;
}
That's it :)
Now the picture is perfect and i can look deeper in the new ST beast ;)
Cheers.
2013-10-17 10:54 AM
Hi :)
I have made a very short video from the 640x480 test on stm429 Disco with VGA. Here it is : Cheers.2013-10-22 8:00 AM
Hi,
Nice video, thanks for posting this. Probably the uGFX project will be interested in this. Giovanni ---2013-10-22 9:51 AM
Hi Giovanni ,
Well , my source are open , i attach it here and if they want it , they can take it ;) I added the 240 x 320 and the 320 x 240 resolution (select it in the 'stm32f429i_discovery_vga.h' file) But , it's based on the 640 x 480 resolution (timing etc ...) If someone know how to double the pixels size directly with the ltdc it will help me to get lower resolution bigger in screen :) Next step will be when i will receive my PCB and can add more SDRAM + SRAM to the stm429 disco ;) If it work it will be open sourced too ... Cheers. Darth. ________________ Attachments : vga_demo_-_2013-10-19-2336.rar : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzmV&d=%2Fa%2F0X0000000bPV%2FSE3p_tT.IocAxIyJHfA329eWMUIRaZ0bvrFL44gZA6Q&asPdf=false2014-10-25 7:12 AM
2014-10-25 7:33 AM