2012-12-07 11:29 AM
Hello! I am develop data aquisition system project on STM32F407. USB flash drive connected to USB host (OTG FS). Project based on sample from stm32_f105-07_f2_f4_usb-host-device_lib.zip. Ide is CooCox 1.6.0.
Data writes to drive by blocks 32kB each 300 ms. After 3-11 writes to drives program hangs on next code: file: usbh_msc_bot.c void USBH_MSC_HandleBOTXfer (USB_OTG_CORE_HANDLE *pdev ,USBH_HOST *phost) { .... case USBH_MSC_DECODE_CSW: URB_Status = HCD_GetURB_State(pdev , MSC_Machine.hc_num_in); /* Decode CSW */ if(URB_Status == URB_DONE) { BOTStallErrorCount = 0; USBH_MSC_BOTXferParam.BOTStateBkp = USBH_MSC_RECEIVE_CSW_STATE; USBH_MSC_BOTXferParam.MSCState = USBH_MSC_BOTXferParam.MSCStateCurrent ; USBH_MSC_BOTXferParam.BOTXferStatus = USBH_MSC_DecodeCSW(pdev , phost); } else if(URB_Status == URB_STALL) { error_direction = USBH_MSC_DIR_IN; USBH_MSC_BOTXferParam.BOTState = USBH_MSC_BOT_ERROR_IN; } HCD_GetURB_State(...) return URB_Status = URB_IDLE, which is not processed. Is it USB Flash drive error? How can I solve the problem? #stm32-usb-msc2012-12-10 4:52 AM
I tried USB HS with embedded PHY on STM32F4. Also I tried 3 types of USB flash drives.
Program still hangs on after 3-11 writes on drive.