cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F407 knowing the bootloader version

ole2399
Associate
Posted on August 20, 2015 at 20:55

Hi !

I have a question regarding the bootloader versions on my STM32F407xx boards :

Is it possible to determin the version of the bootloader a chip contains either from the text printed on the chip or via SWD wires ?

My system can only use the SPI pins for programming so I need to have the v9 bootloader, I presume that the bootloader is in ROM, so it is not upgradeable if I have a chip with the v3 bootloader ?

BR,

Ole A. Torvmark

#bootloader #stm32f407 #version
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on August 20, 2015 at 21:06

You can read the memory on the STM32 using the ST-LINK Utilities, and save it too a file. This includes the ROM, seem to recall there's a specific address to look at, or that it could be gleaned from the binary if not.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..