2019-07-05 04:48 AM
I can't get into boot loader mode (from what i can tell). The PC won't detect the USB port etc.
What I've tried:
Same Circuit and same design 10PCB's are there in that 3 are having this issue. How to solve this Problem?
Thanks in Advance
2019-07-07 08:56 PM
Is there anyone who know the solution?
2019-07-07 09:36 PM
A solution would depend on what's going on with the board and chip.
I'd probably check how the reset is occurring, and try to debug what code is actually running, and upload my own.
USB would be dependent on HSE starting properly.
2019-07-08 11:37 PM
Hi.... If only with USB it is not working means we can consider a code problem but here some PCB's are taking but only one or two giving the issue. Those boards even i tried to dump code through ulink2 debugger but still it is not taking but controller is detecting in Keil 5 software.