cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f4-discovery usb host + bluetooth dongle

spam
Associate II
Posted on December 29, 2011 at 11:29

Hi!

I'm writing the subj code, using btstack project (http://code.google.com/p/btstack) and ST libs.

After fixing couple things in ST libs, I've got partial success (several commands and events are exchanged between host and device).

Now I've encountered rather strange behaviour when trying to enable ACL IN (extra usb input channel). I tracked it down to writing HCCHAR and HCTSIZ regs for the extra channel (which cause the breakdown).

My code is based upon input processing in MSC and HID examples.

Can somebody answer my questions on stm32 usb host rx fifo design?

The first question is: is it ok to access pdev->regs.DFIFO[0] (rather than indexed by the channel accessed) in USB_OTG_ReadPacket() as ST libs do?

#stm32-usb-host
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0