2011-07-22 06:17 AM
Will there be a version of the Flash Loader Demo and the DfuSe Demo available for the STM32F2 series?
I've tried to get both of these to work with a STM3220G Eval board but they don't seem to be compatible, or am I missing the boot code on the STM32F207 device? #stm32f2xx-dfuse-flash-loader2011-07-27 10:23 AM
Hi,
We have uploaded Both SW Demos on our web pages : Then ''Design support'' Cheers, STOne-32.2011-07-28 07:34 AM
Thanks for the update.
The only problem I now have is both the zip files are being blocked by our company firewall, it says the files contain a ''Trojan Virus'' other zip files on the same page are OK just these newly updated ones. Can you check them out.2011-07-28 08:45 AM
Hi,
These zip files contains .exe for installation setup , I believe that your firewall is blocking them since they are .exe. We can not put untrusted contents on our web sites, we have many firewalls and Corporate Anti-virus as well. Cheers, STOne-2011-09-21 08:47 AM
I am wondering if ST plans on supporting Rowley Crossworks. Any information on this?
2011-09-21 09:29 AM
I am wondering if ST plans on supporting Rowley Crossworks. Any information on this?
I think you have that kind of backward. Rowley is responsible for making their own processor and board packages. Although if I understand what you're asking for, I too would probably like to see example projects for Rowley, seeing as how badly the Atollic Lite supports projects. The problem however would be trying to synchronize project files across half-a-dozen platforms, a total nightmare for ST. My first thought would be why can't these alternate platforms import competitive projects, seeing as most are stored in a text or XML format. I've used Rowley with some STR9, STR7 and STM32F1 code, the library code isn't that hard to build a project from scratch.