stm32f207vc usb bulk tramission , only 64bytes can be sent?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-04-10 12:55 AM
Posted on April 10, 2013 at 09:55
I use stm32f207 USB device examples VCP deom .I change the USB CDC device Configuration Descriptor like this
/*Configuration Descriptor*/ 0x09, /* bLength: Configuration Descriptor size */ USB_CONFIGURATION_DESCRIPTOR_TYPE, /* bDescriptorType: Configuration */ USB_CDC_CONFIG_DESC_SIZ, /* wTotalLength:no of returned bytes */ 0x00, 0x01, /* bNumInterfaces: 1 interface */ 0x01, /* bConfigurationValue: Configuration value */ 0x00, /* iConfiguration: Index of string descriptor describing the configuration */ 0xC0, /* bmAttributes: self powered */ 250, /* MaxPower 2 mA */ /*Data class interface descriptor*/ 0x09, /* bLength: Endpoint Descriptor size */ USB_INTERFACE_DESCRIPTOR_TYPE, /* bDescriptorType: */ 0x00, /* bInterfaceNumber: Number of Interface */ 0x00, /* bAlternateSetting: Alternate setting */ 0x02, /* bNumEndpoints: Two endpoints used */ 0xff, /* bInterfaceClass: USER */ 0x00, /* bInterfaceSubClass: */ 0x00, /* bInterfaceProtocol: */ 0x00, /* iInterface: */ //18 /*Endpoint OUT Descriptor*/ 0x07, /* bLength: Endpoint Descriptor size */ USB_ENDPOINT_DESCRIPTOR_TYPE, /* bDescriptorType: Endpoint */ 0x03, /* bEndpointAddress */ 0x02, /* bmAttributes: Bulk */ 0x40, /* wMaxPacketSize: */ 0, 0, /* bInterval: ignore for Bulk transfer */ //25 /*Endpoint IN Descriptor*/ 0x07, /* bLength: Endpoint Descriptor size */ USB_ENDPOINT_DESCRIPTOR_TYPE, /* bDescriptorType: Endpoint */ 0x82, /* bEndpointAddress */ 0x02, /* bmAttributes: Bulk */ 0x40, /* wMaxPacketSize: */ 0, 0 /* bInterval: ignore for Bulk transfer */ //32 and I send function : uint16_t VCP_DataTx (uint8_t* Buf, uint32_t Len) { uint8_t i; for (i=0;i<64;i++) //this number must bemultiple
of 64 ,anyother number wil not be send out. { APP_Rx_Buffer[APP_Rx_ptr_in] = g_ucaHeartbeat; APP_Rx_ptr_in++; /* To avoid buffer overflow */ if(APP_Rx_ptr_in == APP_RX_DATA_SIZE) { APP_Rx_ptr_in = 0; } } return USBD_OK; } #stm32f207-cdc-virtualcom-usb
Labels:
- Labels:
-
USB
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-04-10 10:11 AM
Posted on April 10, 2013 at 19:11
Full speed bulk endpoint limit is 64 bytes. For performance, you want to send full packets.
if you need more granularity, consider another type of end point.Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-04-15 2:13 AM
Posted on April 15, 2013 at 11:13
But when I send 8 bytes ,by calling DCD_EP_Tx(len=8) ,it can not be sent successful?
what wrong with me?