2017-05-29 8:01 AM
I try doing usb device with two bulk endpoint IN/OUT.
All work fine but i lost every first packet on start device. Every new packet work fine, and work fine if i unplug and plug usb cable. And i recevie num of bytes in packet but not his content.
Code on STM32:
USBD_ClassTypeDef USBD_SPI =
{
USBD_SPI_Init, //USBD_MSC_Init,
USBD_SPI_DeInit, //USBD_MSC_DeInit,
NULL, //USBD_MSC_Setup,
NULL, /*EP0_TxSent*/
NULL, /*EP0_RxReady*/
USBD_SPI_DataIn, //USBD_MSC_DataIn,
USBD_SPI_DataOut, //USBD_MSC_DataOut,
NULL, /*SOF */
NULL,
NULL,
USBD_SPI_GetHSCfgDesc,
USBD_SPI_GetFSCfgDesc,
USBD_SPI_GetOtherSpeedCfgDesc,
NULL, //USBD_MSC_GetDeviceQualifierDescriptor,
};
uint8_t buff[100];
uint8_t USBD_SPI_DataOut(USBD_HandleTypeDef *pdev, uint8_t epnum){
printf('Data OUT - %d\r\n', USBD_GetRxCount(pdev, epnum));
printf('TR - %d\r\n', USBD_LL_PrepareReceive(pdev, epnum, buff, 100));
printf('usb_print:0x%02X 0x%02X 0x%02X\r\n', buff[0], buff[1], buff[2]);
return 0;
}
Code what i use to test transfer from linux:
&sharpinclude <stdio.h>
&sharpinclude <stdint.h>
&sharpinclude <libusb-1.0/libusb.h>
libusb_device_handle * dev;
int main(int argc, char **argv){
int x;
char buff[100];
libusb_init(NULL);
dev = libusb_open_device_with_vid_pid(NULL, 0x1234, 0x1234);
if (libusb_kernel_driver_active(dev, 0)){
libusb_detach_kernel_driver(dev, 0);
}
if (libusb_claim_interface(dev, 0) < 0){
printf('Interface error\n');
}
printf('Prepare\r\n');
buff[0] = 0x1; buff[1] = 0x1; buff[2] = 0x1;
libusb_bulk_transfer(dev, 0x01, buff, 3, &x, 0);
buff[0] = 0x2; buff[1] = 0x2; buff[2] = 0x2;
libusb_bulk_transfer(dev, 0x01, buff, 3, &x, 0);
buff[0] = 0x3; buff[1] = 0x3; buff[2] = 0x3;
libusb_bulk_transfer(dev, 0x01, buff, 3, &x, 0);
libusb_close(dev);
libusb_exit(NULL);
}
After start firmware i run transfer data and see in console:
USB RUN
Data OUT - 3TR - 0usb_print:0x00 0x00 0x00Data OUT - 3TR - 0usb_print:0x02 0x02 0x02Data OUT - 3TR - 0usb_print:0x03 0x03 0x03On second tranfer i see normal data:
Data OUT - 3
TR - 0
usb_print:0x01 0x01 0x01
Data OUT - 3
TR - 0
usb_print:0x02 0x02 0x02
Data OUT - 3
TR - 0
usb_print:0x03 0x03 0x03
How i can fix this?
#stm32f103 #lost #usbd #bulkSolved! Go to Solution.
2017-05-31 3:05 AM
I do error in Init fucntion, now i add in end of function this code and all work fine.
USBD_LL_FlushEP(pdev, SPI_EPOUT_ADDR);
USBD_LL_FlushEP(pdev, SPI_EPIN_ADDR);
USBD_LL_PrepareReceive(pdev, SPI_EPOUT_ADDR, buff, 100);
2017-05-31 3:05 AM
I do error in Init fucntion, now i add in end of function this code and all work fine.
USBD_LL_FlushEP(pdev, SPI_EPOUT_ADDR);
USBD_LL_FlushEP(pdev, SPI_EPIN_ADDR);
USBD_LL_PrepareReceive(pdev, SPI_EPOUT_ADDR, buff, 100);