STM32F103: SRAM startup
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-25 4:18 PM
Hi all!
When i try startup my firmware from SRAM on stm32f103RE then nothing..
BOOT1 and BOOT0 is set to 1
Firmware developed on KEIL. Please, look my project settings:
int main(void){
__disable_irq ();
SCB->VTOR = 0x20000000U; __set_MSP(*((volatile uint32_t *) 0x20000000U)); __DSB (); __enable_irq();.....
init's and etc and main programm
......
}
1. I place my compiled firmware over ST-Link Utility on region 0x20000000 (upload dump and check it, all ok),
2. set BOOT1 & BOOT0 = 1,
3. and press RESET. Nothing! =( programm does not work (not blinked).. does not startup
why?
thank
#startup #sram #bootSolved! Go to Solution.
- Labels:
-
Bootloader
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-26 6:33 AM
If the part expects Reset_Handler to be at 0x200001E0 then it is not going to work if your build puts it at 0x20001234 or 0x2000120
Place ' DCD 0xF1E0F85F' at the end of the Vector table space, so it falls at 0x200001E0, to permit operation in this mode.
Look at STM32Cube_FW_F1_V1.6.1\Drivers\CMSIS\Device\ST\STM32F1xx\Source\Templates\gcc\startup_stm32f103xe.s
Attached (use Thread View) is a startup_stm32f103xe.s for Keil modified to permit RAM Booting
________________ Attachments : startup_stm32f103xe.s : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HxYb&d=%2Fa%2F0X0000000azq%2FyPX56Ftsj8dol.KvB31qfnssUB1rqIJjdzYH2U761rQ&asPdf=falseUp vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-25 5:56 PM
As discussed in other threads, over several years, the F1 has some special requirements with the placement of the Reset_Handler code. You will see 'BootRAM' in the GNU/GCC startup.s files for a given low, medium or high density parts. This is effectively a LDR PC,[0x20000004] instruction, but could just be your handler code.
Your main() function really doesn't have to do any of that. SCB->VTOR will be zero at reset, if SRAM is mapped at zero (and you can't change it on the F1, everything will be fine). Usually SCB->VTOR is set in SystemInit()
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-26 12:51 AM
Hi, Clive
thank you for your reply! But i don't understand what to do..
can you more fully explain?
what am I doing wrong in my situation?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-26 1:04 AM
and
when i startup code over Debug (st-link v2) mechanism - all work fine.
programm correct work and trace
i use INI-file:
/*----------------------------------------------------------------------------
Setup() configure PC & SP for RAM Debug *----------------------------------------------------------------------------*/FUNC void Setup (void) { SP = _RDWORD(0x20000000); // Setup Stack Pointer PC = _RDWORD(0x20000004); // Setup Program Counter _WDWORD(0xE000ED08, 0x20000000); // Setup Vector Table Offset Register}FUNC void OnResetExec (void) { // executes upon software RESET
Setup(); // Setup for Running}load %L incremental
Setup(); // Setup for Running
*----------------------------------------------------------------------------*/
what is incorrect when programm startup from hardware boot(BOOT0 & BOOT1 == 1)?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-26 6:17 AM
>>all work fine
No doubt, the debugger completely changes the dynamics, you are fighting specific conditions in the hardware that occur in a real reset.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-26 6:33 AM
If the part expects Reset_Handler to be at 0x200001E0 then it is not going to work if your build puts it at 0x20001234 or 0x2000120
Place ' DCD 0xF1E0F85F' at the end of the Vector table space, so it falls at 0x200001E0, to permit operation in this mode.
Look at STM32Cube_FW_F1_V1.6.1\Drivers\CMSIS\Device\ST\STM32F1xx\Source\Templates\gcc\startup_stm32f103xe.s
Attached (use Thread View) is a startup_stm32f103xe.s for Keil modified to permit RAM Booting
________________ Attachments : startup_stm32f103xe.s : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HxYb&d=%2Fa%2F0X0000000azq%2FyPX56Ftsj8dol.KvB31qfnssUB1rqIJjdzYH2U761rQ&asPdf=falseUp vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-26 2:50 PM
Cool!! it is worked!!
but i place
DCD 0xF1E0F85F with lead zeroes for align end of vector table in my startup
thank you, Clive for it magic