STM32F103 ADC and timer interupt
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-04-19 11:11 AM
Hello!
I want to build a project where i need to do about 3500 readings from a CCD sensor in a short period a time. The signal i want to read has a frequency of about 0.35MHz, which should be fine as long as i use 13.5cycles for sampling time.
The problem is in the intrerupt. Here is how my program works:
- TIM2,3,4 are started in PWM mode, needed for the CCD
In main loop:
- If the reading has been done (it is only done once), send the data over serial port
In interupt of TIM1:
- If the reading hasn t been done already, start ADC, read current pixel and put it in a vector, increment current pixel unless the last pixel has been reached, when then I say that the reading is over.
Unfortunately I do not get anything in the serial output. What can be the problem? Is the interupt routine not called?
Here it is:
void TIM1_UP_IRQHandler(void)
{ /* USER CODE BEGIN TIM1_UP_IRQn 0 */ if(read_all == 0){ HAL_ADC_Start(&hadc1); aTxBuffer[current_pixel] = HAL_ADC_GetValue(&hadc1); if(current_pixel == last_pixel){ read_all = 1; current_pixel = 3; } else current_pixel++; } /* USER CODE END TIM1_UP_IRQn 0 */ HAL_TIM_IRQHandler(&htim1); /* USER CODE BEGIN TIM1_UP_IRQn 1 *//* USER CODE END TIM1_UP_IRQn 1 */
}I have also attached all the code. Thank you!
#stm32f103 #timer-interrupt #hal #adc- Labels:
-
ADC
-
STM32Cube MCU Packages
-
STM32F1 Series
-
TIM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-04-20 10:08 AM
I think I have found the problem, but I do not know hot to fix it.
In main.c I have a variable:
uint16_t testPixel = 1;
uint8_t myChar[5];
In the infinite loop, i just send it every second via UART:
itoa(testPixel, myChar, 10);
HAL_UART_Transmit(&huart1,myChar,sizeof(myChar),10); HAL_Delay(1000);Then in stm32f1xx_it.c I have :
extern testPixel;
[...]
void TIM1_UP_IRQHandler(void)
{ /* USER CODE BEGIN TIM1_UP_IRQn 0 */ testPixel = 2; /* USER CODE END TIM1_UP_IRQn 0 */ HAL_TIM_IRQHandler(&htim1); /* USER CODE BEGIN TIM1_UP_IRQn 1 */ /* USER CODE END TIM1_UP_IRQn 1 */}When I upload the code and test it, I receive over UART '1111', instead of 2.
Here is how the Timer is set-up:
static void MX_TIM1_Init(void)
{TIM_MasterConfigTypeDef sMasterConfig;
TIM_OC_InitTypeDef sConfigOC; TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig;htim1.Instance = TIM1;
htim1.Init.Prescaler = 0; htim1.Init.CounterMode = TIM_COUNTERMODE_UP; htim1.Init.Period = 80-1; htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; htim1.Init.RepetitionCounter = 0; if (HAL_TIM_PWM_Init(&htim1) != HAL_OK) { Error_Handler(); }sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE; if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK) { Error_Handler(); }sConfigOC.OCMode = TIM_OCMODE_PWM1;
sConfigOC.Pulse = 10; sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH; sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH; sConfigOC.OCFastMode = TIM_OCFAST_DISABLE; sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET; sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET; if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_1) != HAL_OK) { Error_Handler(); }sBreakDeadTimeConfig.OffStateRunMode = TIM_OSSR_DISABLE;
sBreakDeadTimeConfig.OffStateIDLEMode = TIM_OSSI_DISABLE; sBreakDeadTimeConfig.LockLevel = TIM_LOCKLEVEL_OFF; sBreakDeadTimeConfig.DeadTime = 0; sBreakDeadTimeConfig.BreakState = TIM_BREAK_DISABLE; sBreakDeadTimeConfig.BreakPolarity = TIM_BREAKPOLARITY_HIGH; sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_DISABLE; if (HAL_TIMEx_ConfigBreakDeadTime(&htim1, &sBreakDeadTimeConfig) != HAL_OK) { Error_Handler(); }HAL_TIM_MspPostInit(&htim1);
}