STM32F051 auto baud feature delay with StdPeriphLib
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-05-16 12:41 AM
I'm trying to use auto baud feature on STM32F051 with STM32F0xx_StdPeriphLib drivers (V1.5.0) to adjust my baud rate to sync-bytes that I receive from another MCU over UART1.
The relevant code looks like that:
/* UART1 already configured and running */
USART_Cmd(USART1, DISABLE);
USART_AutoBaudRateConfig(USART1, USART_AutoBaudRate_StartBit); USART_AutoBaudRateCmd(USART1, ENABLE); USART_Cmd(USART1, ENABLE);The procedure itself works fine, however I encounter delays of ~17 milliseconds until the baud rate adjustment is completed (until UART_FLAG_ABRF becomes set). This delay stays the same no matter how many sync-bytes are sent from the other device during this period.
I tried to use Cuba_Hal Lib for comparison with the following code (taken from an ST example):
huart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_AUTOBAUDRATE_INIT;
huart1.AdvancedInit.AutoBaudRateEnable = UART_ADVFEATURE_AUTOBAUDRATE_ENABLE;huart1.AdvancedInit.AutoBaudRateMode = UART_ADVFEATURE_AUTOBAUDRATE_ONSTARTBIT;
if (HAL_UART_Init(&huart1) != HAL_OK)
{ /* Initialization Error */ Error_Handler();}With this code the auto baud procedure is completed in under 1ms.
Does anybody know why this delay occurs with StdPeriphLib and how I can fix it?
Many thanks in advance!
#rate #stm32f0 #cube_hal #auto-baud #stdperiph_driver- Labels:
-
SPL
-
STM32Cube MCU Packages
-
STM32F0 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-05-16 2:38 AM
Hi
Koscheck.David
,- Have you try to start from ready example under the STM32 standard peripherals library :
STM32F0xx_StdPeriph_Lib_V1.5.0\Projects\STM32F0xx_StdPeriph_Examples\USART\USART_AutoBaudRate
- also try to refer to application note it may help you
-Nesrine-