cancel
Showing results for 
Search instead for 
Did you mean: 

STM324x9I-Eval + LwIP TCP Echo Client not workin

keaven
Associate II
Posted on April 24, 2015 at 23:09

Hello everyone,  I have a project which i want to add the network capabilities .  I am using the SMT324x9I-Eval board to do my first test with the project LwIP_TCP_Echo_Client included in STM32F4Cube 1.5.0.

I am absolutely not able to get a packet from the board on my PC.

I have downloaded EchoTool application and run it on my PC.  In my project I have changed the IP destination to 10.0.0.11 , my source to 10.0.0.10 and put my gateway to 10.0.0.11.

The link in between is a cross-over cable directly into a 2nd network card.  

I am using Wireshark to monitor the NIC and I don't see any pack going in.  Naturally, the echo tool server doesn't get any request.

Anyone has experienced with this demo application or network API on this evaluation board.

Regards, 

#smt32f4x9i-eval-ethernet-lwip
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0