2024-10-09 8:09 AM
I have created a CPP critical section class using stm32_lock_acquire and stm32_lock_release. The main issue is in stm32_lock.h the file #include <cmsis_compiler.h>. The stock version of this file, included with CubeMx won't work if included in a c++ file. Investigating, I found that if I move the cmsis_compiler.h include in to the extern "C" block, it works just fine. Am I misusing stm32_lock? or is this a suitable way to create a critical section in cpp?
Before change - won't compile because cmsis_complier.h or something it includes cannot complied with a c++ compiler.
#ifndef __STM32_LOCK_H__
#define __STM32_LOCK_H__
/* Includes ------------------------------------------------------------------*/
#include <stdint.h>
#include <stddef.h>
#include <cmsis_compiler.h>
#ifndef STM32_THREAD_SAFE_STRATEGY
#define STM32_THREAD_SAFE_STRATEGY 2 /**< Assume strategy 2 if not specified */
#endif /* STM32_THREAD_SAFE_STRATEGY */
#ifdef __cplusplus
extern "C" {
#endif /* __cplusplus */
/* Function prototypes -------------------------------------------------------*/
void Error_Handler(void);After change - now it will compile fine since the include is inside the extern "C" block.
#ifndef __STM32_LOCK_H__
#define __STM32_LOCK_H__
/* Includes ------------------------------------------------------------------*/
#include <stdint.h>
#include <stddef.h>
#ifndef STM32_THREAD_SAFE_STRATEGY
#define STM32_THREAD_SAFE_STRATEGY 2 /**< Assume strategy 2 if not specified */
#endif /* STM32_THREAD_SAFE_STRATEGY */
#ifdef __cplusplus
extern "C" {
#endif /* __cplusplus */
#include <cmsis_compiler.h>
/* Function prototypes -------------------------------------------------------*/
void Error_Handler(void);
Header file
#ifndef __CRITICAL_SECTION_H__
#define __CRITICAL_SECTION_H__
#include "stm32_lock.h"
namespace Library
{
/*
CriticalSection
---
Usage:
void someInterruptSensitiveCode(void)
{
//not interrupt sensitive code
{
//this disables interrupts in the constructor
//the name of the variable is not important.
Library::CriticalSection newSection;
//interrupts are now disabled
//you may change variables without fear of being interrupted
}//interrupts are re-enabled when newSection goes out of context or {}
//not interrupt sensitive code
}
*/
class CriticalSection
{
public:
CriticalSection();
~CriticalSection();
private:
LockingData_t lock = LOCKING_DATA_INIT;
};
} // namespace Library
#endif //__CRITICAL_SECTION_H__CPP file
#include "CriticalSection.h"
#include "stm32_lock.h"
namespace Library
{
CriticalSection::CriticalSection()
{
// thread and interrupt safe lock
stm32_lock_acquire(&lock);
}
CriticalSection::~CriticalSection()
{
// thread and interrupt safe lock
stm32_lock_release(&lock);
}
} // namespace Library