2025-10-15 9:16 AM
Hi,
I'm on a applicaiton involving USBX MSC and FileX.
The final memory for the application is a NOR flash so I also use LevelX.
Acutally, I'm working on a nucleo-U575ZI-Q without NOR flash so I use NOR Simulator on LevelX.
My problem is that a file created with FileX is detected by windows, have the right number of bytes but data are wrong.
My program do this:
1) FileX format the device
2) FileX create the file STM32.TXT and put the data "This is FileX working on STM32". I can see this data on the RAM
3) FileX close and open the file STM32.TXT and I can read the text
4) FileX close the media.
5) USBX open the media and on Windows I see the file STM32.TXT but data are not correct. It's like if this data comes from another part on my RAM.
When the device is connected to a computer, I can create new file, write on it then unplug / plug USB and the new file is still here. I can also edit STM32.TXT.
Has somebody an idea about why FileX can read right data but windows doesn't read right data even if the device is mounted.
Thanks for help !
Solved! Go to Solution.
2025-11-24 11:22 PM
Hello Dams,
Can you please share your project if it is possible. I am trying learning this topics.
Thank you
Regards.