2025-12-09 12:25 AM - last edited on 2025-12-09 12:36 AM by Imen.D
I have NUCLEO-WB05K/NUCLEO-WB07CC/NUCLEO-WB09KE only the NUCLEO-WB09KE can be connected to with Software Reset mode.
The NUCLEO-WB05K/NUCLEO-WB07CC boards have the above error on connect.
The Hardware Reset mode doesn't work with the NUCLEO-WB09KE (or the other boards).
All STLink firmware up to date - not many jumper options to get wrong on these boards.
Windows 11.
Solved! Go to Solution.
2025-12-09 12:42 AM
Hello @mpj1
You might have encountered the issue described in this article:
Establishing the initial connection with NUCLEO-WB05KZ, 7CC, and 9KE boards
So, try entering bootloader mode using the correct jumper settings to recover the boards.
2025-12-09 12:42 AM
Hello @mpj1
You might have encountered the issue described in this article:
Establishing the initial connection with NUCLEO-WB05KZ, 7CC, and 9KE boards
So, try entering bootloader mode using the correct jumper settings to recover the boards.
2025-12-09 1:02 AM
Setting the JP1 to BOOTLoader and and connection mode to Normal/Hot plug I've manage to connect by holding the reset button and connecting as soon as I can when releasing the reset button.....