2013-09-10 9:55 AM
I was wondering if there is any DFU software compatible with Linux that can be used to upgrade the firmware of an STM32F405 using the USB interface? Essentially I'm looking a Linux version of the Windows DfuSe software. Thanks in advance.
#dfu #firmware #stm32 #lmgtfy #linux2013-09-10 10:05 AM
http://dfu-util.gnumonks.org/dfuse.html
2013-09-10 12:10 PM
Thanks!
2013-12-20 6:46 AM
i'm working on a version that bases off some earlier work for atmel avr32 devices. It is being developed on ubuntu. So far write works but not read.
2013-12-23 12:49 AM
inman, this was also done before, by Antonio Borneo. Please see
http://article.gmane.org/gmane.comp.debugging.openocd.devel/21278