2020-06-18 2:35 AM
Serial port interrupts are firing continuously, so that the application code does not run.
I'm using an STM32H743, on the Nucleo board.
Initially, USART3 worked properly for a few weeks, then failed in this manner. I then moved to USART1, which worked for a few weeks, then also failed like this. The testing was done with RX grounded and TX left unconnected. The same results are obtained if RX is left floating.
The following flags are observed as set on each interrupt:
BUSY, CM, CTS, EOB, IBD, NE, ORE, REACK, RTO, RXFF, SBK, TXFT, WKUP.
I am only looking for RXNE, TC, and TXE. (For receiving bytes and sending bytes.)
What can I do to stop USART1_IRQHandler() being called continuously?
P.S. I configure the port with the (mostly) generated:
static void MX_USART1_UART_Init(void)
{
/* USER CODE BEGIN USART1_Init 0 */
/* USER CODE END USART1_Init 0 */
LL_USART_InitTypeDef USART_InitStruct = {0};
LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
/* Peripheral clock enable */
LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_USART1);
LL_AHB4_GRP1_EnableClock(LL_AHB4_GRP1_PERIPH_GPIOB);
/**USART1 GPIO Configuration
PB15 ------> USART1_RX
PB6 ------> USART1_TX
*/
GPIO_InitStruct.Pin = LL_GPIO_PIN_15;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
GPIO_InitStruct.Alternate = LL_GPIO_AF_4;
LL_GPIO_Init(GPIOB, &GPIO_InitStruct);
GPIO_InitStruct.Pin = LL_GPIO_PIN_6;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
GPIO_InitStruct.Alternate = LL_GPIO_AF_7;
LL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/* USART1 interrupt Init */
NVIC_SetPriority(USART1_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),0, 0));
NVIC_EnableIRQ(USART1_IRQn);
/* USER CODE BEGIN USART1_Init 1 */
//return;
/* USER CODE END USART1_Init 1 */
USART_InitStruct.PrescalerValue = LL_USART_PRESCALER_DIV1;
USART_InitStruct.BaudRate = 115200; //38400;
USART_InitStruct.DataWidth = LL_USART_DATAWIDTH_8B;
USART_InitStruct.StopBits = LL_USART_STOPBITS_1;
USART_InitStruct.Parity = LL_USART_PARITY_NONE;
USART_InitStruct.TransferDirection = LL_USART_DIRECTION_TX_RX;
USART_InitStruct.HardwareFlowControl = LL_USART_HWCONTROL_NONE;
USART_InitStruct.OverSampling = LL_USART_OVERSAMPLING_16;
LL_USART_Init(USART1, &USART_InitStruct);
LL_USART_SetTXFIFOThreshold(USART1, LL_USART_FIFOTHRESHOLD_1_8);
LL_USART_SetRXFIFOThreshold(USART1, LL_USART_FIFOTHRESHOLD_1_8);
LL_USART_DisableFIFO(USART1);
LL_USART_ConfigAsyncMode(USART1);
/* USER CODE BEGIN WKUPType USART1 */
/* USER CODE END WKUPType USART1 */
LL_USART_Enable(USART1);
/* Polling USART1 initialisation */
while((!(LL_USART_IsActiveFlag_TEACK(USART1))) || (!(LL_USART_IsActiveFlag_REACK(USART1))))
{
}
/* USER CODE BEGIN USART1_Init 2 */
LL_USART_EnableIT_RXNE(USART1);
/* USER CODE END USART1_Init 2 */
}and I catch the flags with:
/*
* @brief Should be called only by UART/USARTx_IRQHandler()
*/
void port_irq_handler(struct port *port)
{
if (LL_USART_IsActiveFlag_ABR(port->usart)) {
port->stats.abr++;
}
if (LL_USART_IsActiveFlag_ABRE(port->usart)) {
port->stats.abre++;
}
if (LL_USART_IsActiveFlag_BUSY(port->usart)) {
port->stats.busy++;
}
if (LL_USART_IsActiveFlag_CM(port->usart)) {
port->stats.cm++;
}
if (LL_USART_IsActiveFlag_CTS(port->usart)) {
port->stats.cts++;
}
if (LL_USART_IsActiveFlag_EOB(port->usart)) {
port->stats.eob++;
}
if (LL_USART_IsActiveFlag_FE(port->usart)) {
port->stats.fe++;
}
if (LL_USART_IsActiveFlag_IDLE(port->usart)) {
port->stats.idle++;
LL_USART_ClearFlag_IDLE(port->usart);
}
if (LL_USART_IsActiveFlag_LBD(port->usart)) {
port->stats.lbd++;
}
if (LL_USART_IsActiveFlag_NE(port->usart)) {
port->stats.ne++;
}
if (LL_USART_IsActiveFlag_ORE(port->usart)) {
port->stats.ore++;
}
if (LL_USART_IsActiveFlag_PE(port->usart)) {
port->stats.pe++;
}
if (LL_USART_IsActiveFlag_REACK(port->usart)) {
port->stats.reack++;
}
if (LL_USART_IsActiveFlag_RTO(port->usart)) {
port->stats.rto++;
}
if (LL_USART_IsActiveFlag_RWU(port->usart)) {
port->stats.rwu++;
}
if (LL_USART_IsActiveFlag_RXFF(port->usart)) {
port->stats.rxff++;
}
if (LL_USART_IsActiveFlag_RXFT(port->usart)) {
port->stats.rxft++;
}
if (LL_USART_IsActiveFlag_RXNE(port->usart)) {
port->stats.rxne++;
uint8_t b = LL_USART_ReceiveData8(port->usart);
circbuf_push(&port->rxcircbuf, b);
}
if (LL_USART_IsActiveFlag_RXNE_RXFNE(port->usart)) {
port->stats.rxne_rxfne++;
}
if (LL_USART_IsActiveFlag_SBK(port->usart)) {
port->stats.sbk++;
}
if (LL_USART_IsEnabledIT_TC(port->usart)) {
if (LL_USART_IsActiveFlag_TC(port->usart)) {
port->stats.tc++;
LL_USART_DisableIT_TC(port->usart);
port_run(port);
}
}
if (LL_USART_IsActiveFlag_TC(port->usart)) {
port->stats.tc++;
if (port->txbusy) {
port->txbusy = 0;
} else {
Error_Handler();
}
LL_USART_DisableIT_TC(port->usart);
}
if (LL_USART_IsActiveFlag_TCBGT(port->usart)) {
port->stats.tcbgt++;
}
if (LL_USART_IsActiveFlag_TEACK(port->usart)) {
port->stats.teack++;
}
if (LL_USART_IsActiveFlag_TXE(port->usart)) {
port->stats.txe++;
if (LL_USART_IsEnabledIT_TXE(port->usart)) {
LL_USART_DisableIT_TXE(port->usart);
port_run(port);
}
}
if (LL_USART_IsActiveFlag_TXE_TXFNF(port->usart)) {
port->stats.txe_txfnf++;
}
if (LL_USART_IsActiveFlag_TXFE(port->usart)) {
port->stats.txfe++;
}
if (LL_USART_IsActiveFlag_TXFT(port->usart)) {
port->stats.txft++;
}
if (LL_USART_IsActiveFlag_UDR(port->usart)) {
port->stats.udr++;
}
if (LL_USART_IsActiveFlag_WKUP(port->usart)) {
port->stats.wkup++;
}
if (LL_USART_IsActiveFlag_nCTS(port->usart)) {
port->stats.ncts++;
}
}
Solved! Go to Solution.
2021-02-03 12:02 PM
Well, that's Cube for you.
By using the clicky and/or "library", you gave up control and accepted that somebody else decides what's good for you.
But thanks for chiming in with the warning.
JW