2013-01-17 1:23 AM
Hi guys,
I'm working for the first time on a STM3210C eval. I have to store files on the SD card included in the STM card. So I added FatFs to my project. As FatFs is platform independant, I have to find a compatible SD driver which can provide several functions : disk_ioctl(), disk_read(), etc... I've searched on the Internet and tried to add many drivers, without success. Has someone a SD card driver for STM3210C eval which is compatible with FatFs, and a short ''how to do'' would be great :) thanks, Nicolas #stm3210c-eval-fatfs-sd-driver2013-01-18 1:25 AM
The attached file may help you. also on the following an example based on STM32F2 and STM32F4.
STM32F2 and STM32F4 demonstration builder platform: http://www.st.com/internet/mcu/product/252jsp ________________ Attachments : diskio.c : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0tK&d=%2Fa%2F0X0000000bgu%2FhRMSD1bC2TDMV6ATzYZyDF3utsyZo85baXvpfSyDPSw&asPdf=false2013-01-18 7:43 AM
And here's another example, this was from a project which ran on the STM3210C eval board.
Cheers, Mark ________________ Attachments : disk_io.c : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtW3&d=%2Fa%2F0X0000000aR8%2Fhi0lzhTc.XQ.fM7U3IVGXWWdSTPy8VpIkDrbhvOULjw&asPdf=falsediskio.h : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtII&d=%2Fa%2F0X0000000aLB%2FtXeVc8krFLmakC39JJZFCEiyj8amUvXhzFFXQSq3XQI&asPdf=falsesdcard.c : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtW8&d=%2Fa%2F0X0000000aR9%2F4cFtJ5ITDcA2m2Nff0A8vzhlXJidtE59t7Abbix6UBo&asPdf=falsesdcard.h : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtWD&d=%2Fa%2F0X0000000aRA%2FdcR0xa.nrzTRzVz9E.lwZnpR_M1KxGgGJd5CoFZeJzU&asPdf=false2013-01-21 2:44 AM
Thank you for your answers.
@mclean.mark : ''global.h'' in the c files is not recognized by my compiler. I managed to compilate by replacing ''global.h by : #include ''stm32f10x_sdio.h'' #include ''stm32f10x_dma.h'' #include ''stm32f10x_rcc.h'' #define NULL ((void *)0) I modified SDIO_configuration in sdcard.c : static void SDIO_Configuration(void) { GPIO_InitTypeDef GPIO_InitStructureA; GPIO_InitTypeDef GPIO_InitStructureC; RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOC, ENABLE); GPIO_InitStructureC.GPIO_Pin = GPIO_Pin_10 | GPIO_Pin_11 | GPIO_Pin_12; GPIO_InitStructureC.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructureC.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOC, &GPIO_InitStructureC); /* Configure PD.02 CMD line */ GPIO_InitStructureA.GPIO_Pin = GPIO_Pin_4; GPIO_InitStructureA.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructureA.GPIO_Mode = GPIO_Mode_Out_PP; GPIO_Init(GPIOA, &GPIO_InitStructureA); } But it still doesn't work when I do in the main : FIL fil_obj; FATFS fs[1]; FRESULT FRes; disk_initialize(0); f_mount(0, &fs[0]); f_open(&fil_obj, ''0:whatever.txt'', FA_OPEN_ALWAYS | FA_READ); f_close(&fil_obj); f_mount(0, NULL); Note : I use the firmware 3.3.0, and the processor is a STM3210f107VC Some ideas ?2013-01-21 2:51 AM
your SDIO init is not correct it should be more like this
void SD_LowLevel_Init(void){ GPIO_InitTypeDef GPIO_InitStructure; /*!< GPIOC and GPIOD Periph clock enable */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC | RCC_APB2Periph_GPIOD | SD_DETECT_GPIO_CLK, ENABLE); /*!< Configure PC.08, PC.09, PC.10, PC.11, PC.12 pin: D0, D1, D2, D3, CLK pin */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8 | GPIO_Pin_9 | GPIO_Pin_10 | GPIO_Pin_11 | GPIO_Pin_12; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOC, &GPIO_InitStructure); /*!< Configure PD.02 CMD line */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2; GPIO_Init(GPIOD, &GPIO_InitStructure); /*!< Configure SD_SPI_DETECT_PIN pin: SD Card detect pin */ GPIO_InitStructure.GPIO_Pin = SD_DETECT_PIN;// GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPU; // Pull up on board GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_Init(SD_DETECT_GPIO_PORT, &GPIO_InitStructure); /*!< Enable the SDIO AHB Clock */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_SDIO, ENABLE); /*!< Enable the DMA2 Clock */ RCC_AHBPeriphClockCmd(SD_SDIO_DMA_CLK, ENABLE);}2013-01-21 3:14 AM
ignore my last post your not using SDIO interface.
2013-01-21 4:48 AM
Some ideas ?
disk_initialize() is called internally by FatFs. FatFs returns errors, examine them and don't continue to plough forward if it fails. Use a debugger and scope if you need to understand what's happening. Debug and test the SD read/write routines outside of FatFs, if they don't work standalone, they aren't going to work when integrated, and debugging is harder.