RTOS f_mount() Heap Leak in HEAP_1 model
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-01-20 2:53 AM
I have a 1 second loop that tries to mount the SD card, It repeatedly calls f_mount() until an SD is detected, however, I've noticed that there is a semaphore created each time f_mount() is called which is not deleted in HEAP_1 mode. So after some time all the heap is consumed. I realise that using HEAP_1 mode objects aren't freed, so should I be doing this another way if I want to mount the disk if its ejected and re-inserted?
This is the call the creates the smaphore:
#if _FS_REENTRANT
/*------------------------------------------------------------------------*/
/* Create a Synchronization Object */
/*------------------------------------------------------------------------*/
/* This function is called in f_mount() function to create a new
/ synchronization object, such as semaphore and mutex. When a 0 is returned,
/ the f_mount() function fails with FR_INT_ERR.
*/
int ff_cre_syncobj ( /* 1:Function succeeded, 0:Could not create the sync object */
BYTE vol, /* Corresponding volume (logical drive number) */
_SYNC_t *sobj /* Pointer to return the created sync object */
)
{
int ret;
#if _USE_MUTEX
#if (osCMSIS < 0x20000U)
osMutexDef(MTX);
*sobj = osMutexCreate(osMutex(MTX));
#else
*sobj = osMutexNew(NULL);
#endif
#else
#if (osCMSIS < 0x20000U)
osSemaphoreDef(SEM);
*sobj = osSemaphoreCreate(osSemaphore(SEM), 1);
#else
*sobj = osSemaphoreNew(1, 1, NULL);
#endif
#endif
ret = (*sobj != NULL);
return ret;
}
And this is the code that calls osSemaphoreDelete() which is ignored in HEAP_1 mode:
/*------------------------------------------------------------------------*/
/* Delete a Synchronization Object */
/*------------------------------------------------------------------------*/
/* This function is called in f_mount() function to delete a synchronization
/ object that created with ff_cre_syncobj() function. When a 0 is returned,
/ the f_mount() function fails with FR_INT_ERR.
*/
int ff_del_syncobj ( /* 1:Function succeeded, 0:Could not delete due to any error */
_SYNC_t sobj /* Sync object tied to the logical drive to be deleted */
)
{
#if _USE_MUTEX
osMutexDelete (sobj);
#else
osSemaphoreDelete (sobj);
#endif
return 1;
}
osStatus_t osSemaphoreDelete (osSemaphoreId_t semaphore_id) {
SemaphoreHandle_t hSemaphore = (SemaphoreHandle_t)semaphore_id;
osStatus_t stat;
#ifndef USE_FreeRTOS_HEAP_1
if (IS_IRQ()) {
stat = osErrorISR;
}
else if (hSemaphore == NULL) {
stat = osErrorParameter;
}
else {
#if (configQUEUE_REGISTRY_SIZE > 0)
vQueueUnregisterQueue (hSemaphore);
#endif
stat = osOK;
vSemaphoreDelete (hSemaphore);
}
#else
stat = osError;
#endif
return (stat);
}
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0