2018-11-07 12:59 PM
For STM32F746 Discovery. This seems to work with buffers from 1 to 20 or so. If you have comments I am happy hear them. Unfortunately for UART6, because that is easily available in Discovery board.
I used UART_TwoBoards_ComIT example as a basis, so you need to replace its main.c with this.
#include "main.h"
UART_HandleTypeDef UartHandle;
__IO ITStatus UartReady = RESET;
__IO uint32_t UserButtonStatus = 0; /* set to 1 after User Button interrupt */
/* Buffer used for reception */
volatile uint8_t aRxBuffer[52];
volatile uint8_t total[300];
void SystemClock_Config(void);
static void Error_Handler(void);
static void CPU_CACHE_Enable(void);
volatile int counte;
int lask=0;
int aa=0;
int main(void)
{
/* Enable the CPU Cache */
CPU_CACHE_Enable();
HAL_Init();
SystemClock_Config();
/* Configure LED1 */
BSP_LED_Init(LED1);
counte=0;
UartHandle.Instance = USARTx;
UartHandle.Init.BaudRate = 9600;
UartHandle.Init.WordLength = UART_WORDLENGTH_8B;
UartHandle.Init.StopBits = UART_STOPBITS_1;
UartHandle.Init.Parity = UART_PARITY_NONE;
UartHandle.Init.HwFlowCtl = UART_HWCONTROL_NONE;
UartHandle.Init.Mode = UART_MODE_TX_RX;
UartHandle.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if(HAL_UART_DeInit(&UartHandle) != HAL_OK)
{
Error_Handler();
}
if(HAL_UART_Init(&UartHandle) != HAL_OK)
{
Error_Handler();
}
UartReady = SET;
while (1)
{
while (UartReady == SET)
{
if(HAL_UART_Receive_IT(&UartHandle, (uint8_t *)aRxBuffer, 1) != HAL_OK)
{
Error_Handler();
}
UartReady = RESET;
BSP_LED_Toggle(LED1);
}
while(counte>27)
{
BSP_LED_Toggle(LED1);
HAL_Delay(100);
/* Infinite loop */
}
}
}
void SystemClock_Config(void)
{
RCC_ClkInitTypeDef RCC_ClkInitStruct;
RCC_OscInitTypeDef RCC_OscInitStruct;
HAL_StatusTypeDef ret = HAL_OK;
/* Enable HSE Oscillator and activate PLL with HSE as source */
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 25;
RCC_OscInitStruct.PLL.PLLN = 432;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = 9;
ret = HAL_RCC_OscConfig(&RCC_OscInitStruct);
if(ret != HAL_OK)
{
while(1) { ; }
}
ret = HAL_PWREx_EnableOverDrive();
if(ret != HAL_OK)
{
while(1) { ; }
}
RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2);
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
ret = HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_7);
if(ret != HAL_OK)
{
while(1) { ; }
}
}
void HAL_UART_TxCpltCallback(UART_HandleTypeDef *UartHandle)
{
/* Set transmission flag: transfer complete */
}
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *UartHandle)
{
while (aa<1)
{
total[counte]=aRxBuffer[aa];
counte++;
aa++;
}
UartReady = SET;
aa=0;
}
void HAL_UART_ErrorCallback(UART_HandleTypeDef *UartHandle)
{
/* Set transmission flag: transfer complete */
HAL_Delay(1000);
BSP_LED_Toggle(LED1);
}
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
if(GPIO_Pin == KEY_BUTTON_PIN)
{
UserButtonStatus = 1;
}
}
static void Error_Handler(void)
{
/* Turn LED1 on */
BSP_LED_On(LED1);
while(1)
{
/* Error if LED1 is slowly blinking (1 sec. period) */
BSP_LED_Toggle(LED1);
HAL_Delay(1000);
}
}
static void CPU_CACHE_Enable(void)
{
/* Enable I-Cache */
SCB_EnableICache();
/* Enable D-Cache */
SCB_EnableDCache();
}
void assert_failed(uint8_t* file, uint32_t line)
{
/* Infinite loop */
while (1)
{
}
}In time I plan to test end of line /n to catch whole sentences but that is an other story. And finally, using a loop of one is silly, I know.
2018-11-08 5:07 AM
Not much comments. When I searched for receiving with UART and using HAL API, I found only a lot of questions but not much good answers. This works. But still I would like hear if some else has tried this.
2018-11-08 5:33 AM
Your buffer/method looks to be poorly bounded, I'd approach this differently.
>>Not much comments.
I get tired of repeating myself. Once upon a time I had a thread "GPS NMEA Decoder Demo for STM32F746G-DISCO" and a similar one for the L4 that demonstrated an efficient interrupt based line parser.
The forum migration seems to have destroyed a lot of content. The HAL USART implementation is overly heavy and convoluted, when it is easier to code a better solution, one usually does.
2018-11-08 5:46 AM
Check the F091 thread, I showed some Uart code there...
2018-11-08 5:59 AM
> The HAL USART implementation is overly heavy and convoluted, when it is easier to code a better solution, one usually does.
Which makes more experienced users ignore threads related to HAL/Cube - based UART code.