2017-11-23 4:09 AM
Hi everyone,
I'm developing an HID Host application to comunicate with a own device and I'm using the NUCLEO-F446ZE board.
At the start I tried to use the HID_Standalone application in the STM32CubeF4 firmware package and then, I tried to develop a new application with STMCube configurator.In both case I tried to connect (with OTG connector) 3 different type of mouse and 1 keyboard and no all device are able to comunicate with microcontroller:
All the previous devices are tested with PC and work fine and the board are powerd with external source.
What can be the problem and how can I fix it?
Thanks in advance
#usb-hid #usb-host #stmcube-f4-usb #middlewareSolved! Go to Solution.
2018-01-26 7:56 AM
I have applied the
pavel_a
patch suggested inhttps://community.st.com/0D70X000006SyJZSA0
and seems the USB stack works fine! I hope, as soon as possible, ST release the USB stack with these fixs.Regards
2017-12-05 7:56 AM
Nobody can help me?
I continued debugging code and I saw the problem is the device send to the host STALL handshake when the host try to enumerate or, with a custom device different from previosus devices, when it call SetReport or GetReport.
I read on-line that the device return STALL handshake when endpoint is in HALT state.
What could be the problem?
2017-12-05 10:35 AM
>>Nobody can help me?
Tried your local ST Micro office, and the FAE's on staff there?
2017-12-06 1:24 AM
I contacted ST online support but I didn't receive replies.
This morning I have sent an email to my local FAE and I'm waiting an answer.
What do you mean with 'FAE's on staff there'?
Thanks in advance.
2017-12-11 4:22 AM
Hi ​,
Do you confirm that you have same behavior in both cases: when using
HID_Standalone application in the STM32CubeF4 firmware package or when generating your own code with STM32CubeMX?
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2017-12-11 6:23 AM
Yes I confirm that I have same behavior in both cases. I had to make some changes in the HID_Standalone beacause I haven't the TFT shield but this shouldn't cause issues for USB because the changes, are only in the code for TFT shield.
I developed my application with STM32CubeMX and following the HID_Standalone application.
This mornig I have seen that in the NUCLEO-446ZE there wasn't the xtal and the clock was provided by MCO (this could be a problem for USB that want a accurate clock).
I have mounted one 24MHz xtal, I have followed all the steps of 6.8.1 section of UM1974 and set the correct parameters in the STM32CubeMX with Clock Configuration but the problem has not be solved.
2017-12-18 5:05 AM
Hi everyone,
I have the same problem on a custom board based on STM32F429.
I need to connect a USB keyboard to the system as an input device and some works and some don't.
I tried with 6 different keyboard and only two works (a Dell and HP keyboard) : all the others aren't recognized by the system.
I'm facing the same problem of the Trust Mouse 16144 in the original message of this thread (
USBH_Process state machine in the usbh_core.c file of the Middlewares, blocks in the HOST_ENUMERATION state).
The thread is marked as Resolved but I can't see any solution.
2017-12-19 5:03 AM
Yes, I contacted to change the status but nothing.
The problem isn't solved, I also contacted the on-line support but no solutions have been found.
I don't know if for you can be useful but I have added other details in further reply to Amel N.
2017-12-19 6:27 AM
Hello,
Please note that this question is marked for action just to keep tracking for it: it means we are working on it.
I shared the case with our USB experts who should help to do a deeper analysis.
luca.giuliodori
, could you please share OLS ticket number? We need it to avoid duplicating effort.I will make a branch for the post where you are reporting possible bugs in stm32f4xx_II_usb; it should be better to manage it separately.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2017-12-19 9:39 AM
Ok no problem and thank you for your attention. Where can I find
OLS ticket number?