cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with using USB_OTG_FS and USB_OTG_HS (internal) as Mass Storage Host Class

MB1
Associate

Hi,

I generated a project for STM32F429 in CubeMX 4.27.0 using USB_OTG_FS and USB_OTG_HS (internal) as Mass Storage Host Class. But in the generated project, USB_OTG_HS does not work in (FS) mode. While searching for the error, I noticed that in the ffconf.h file, the hUSB_Host tag is assigned only to hUsbHostFS. In the projects generated in CubeMX 5.0, this is the same.

How to fix the error? I need to work with both USB_OTG_HS and USB_OTG_FS simultaneously.

Thank you in advance.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0