2017-01-30 6:59 AM
Hi all! I'm trying to interface a STM32F7 with an 32 GB SDHC card, using the latest firmware libraries.
I'm using a STM32f746G DISCO and I started from the project under STM32746G-Discovery/Appllications/FatFs/FatFs_uSD..
I wrote a simple function and I executed it in the main after linking the driver and mounting the disk, to test reliability. The function is the following, where I write 1000 files in a loop..
ErrorStatus Test(void) { FIL MyFile; FRESULT res; uint32_t byteswritten; TCHAR StringPath[100] = {0}; cont=0; while(cont < 1000) { sprintf((char*)StringPath,'File%d.fil', cont); res = f_open(&MyFile, StringPath, FA_CREATE_ALWAYS | FA_WRITE); if(res !=FR_OK) return ERROR; res = f_write(&MyFile, (void*)TempBuffer, sizeof(TempBuffer), (void *)&byteswritten); if((byteswritten == 0) || (res != FR_OK)) { return ERROR; } f_close(&MyFile); cont++; } return SUCCESS; }�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�? TempBuffer is a global uint8_t buffer of size 51
The problem is that after correctly writing some files, f_write returns 'FR_DISK_ERR' and I can't understand why..Decreasing the buffer's size seems to allow a bigger number of files to be written before the error, but it doesn't solve it...
Actually the problem is part of a much bigger project, but since I'm trying to understand what's wrong, I'm trying to keep things as simple as possible. That's why I took a STM32Cube project and left it untouched apart from the function I wrote.. But I really can't get the point of this problem anymway..Any idea?
I'm not using DMA, nor SD peripheral interrupt (as in the example).. The file ffconf.h is left untouched with_USE_LFN = 0, _USE_STRFUNC=2,_MIN_SS=__MAX_SS=5. Systick priority is as low as possible (0x0F).. #sd #fatfs #sd-card #stm32f7 #stm32 #stm32cube Note: this post was migrated and contained many threaded conversations, some content may be missing.2017-02-20 2:02 AM
Hi Nemui,
Thanks for your posts ! I'm very grateful !
I tried your code spirit in order to make my Micron 32Gb eMMC work correctly.
However , I get some strange behavior. In fact, when powering on the eMMC a CMD_RSP_TIMEOUT error occurs
randomly ( sometimes I get no error ) . I checked my Initialization clock frequency and was set to be less than 400KHz.
This same error (
CMD_RSP_TIMEOUT ) occurs also when I try to process write operation ( sometimes it doesn't occur ) !
If a SW command passes one time why it'snt the case all the time ?
What could be the problem ?
please I need help
:(
2017-02-20 4:11 AM
Hi Elliot,
I found
an interesting
solution to my problem
with the
SD
card on
STM32F7
.
I changed the
settings
edges of the
CLK
signal.
STM32CubeMX
generates
automatically the
rising edge
. I used the
falling edge
. It is necessary to change the settingsin two files main.c and stm32f7xx_hal_sd.c. I use the STM32Cube_FW_F7_V1.5.1.
main.c
static void MX_SDMMC1_SD_Init(void)
{hsd1.Instance = SDMMC1;
hsd1.Init.ClockEdge = SDMMC_CLOCK_EDGE_RISING; // <<<< change to SDMMC_CLOCK_EDGE_FALLING....stm32f7xx_hal_sd.c
HAL_SD_ErrorTypedef HAL_SD_Init(SD_HandleTypeDef *hsd, HAL_SD_CardInfoTypedef *SDCardInfo)
{ __IO HAL_SD_ErrorTypedef errorstate = SD_OK; SD_InitTypeDef tmpinit; /* Allocate lock resource and initialize it */ hsd->Lock = HAL_UNLOCKED; /* Initialize the low level hardware (MSP) */ HAL_SD_MspInit(hsd); /* Default SDMMC peripheral configuration for SD card initialization */ tmpinit.ClockEdge = SDMMC_CLOCK_EDGE_RISING; // <<<< change to SDMMC_CLOCK_EDGE_FALLING........
Petr
2017-02-20 4:23 AM
Hi Petr,
thanks for your response ! I will implement it then I will be back to give my feedback.
Otherwise , concerning the CMD_RSP_TIMEOUT error isn't a recurrent issue ? I didn't find a lot of information about it .
thanks,
Elliot
2017-02-20 5:39 PM
Dear Eliot,
You said 'sometimes it doesn't occur'...
Same situation I met,it doesn't match 'clock line impedance'.STM32 can goes up to about 50MHz SDIO clock by ultra-fast rizing/falling toggling,
thus often generates tremendous ringing despite any clock frequency for unmached impedance pcb.To suppress ringings,insert series resistor(22~47ohm) on nearby STM32's SDIO_CK.
See also attached application note for more detail.
Best regards,
Nemui. ________________ Attachments : tnfc35_emmc_pcb_design_guide.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyuE&d=%2Fa%2F0X0000000bDj%2FUzH2U2i_wIDpkZrxRbRlZmCbRaU0mjx6zR3eezMovzU&asPdf=false2017-02-22 2:17 AM
Hi Nemui ,
Thanks a lot for your response !
I go back to check and I will let you what have been changed .
Thanks again !
kind and best regards,
2017-02-23 7:23 AM
Hi
Nemui,
I have checked my SDMMC_CLK line and I found that there's a 22 Ohm resistance . Is it enough ? Should I add another serial resistance?
I have to mention that with the STM32L486RG microcontroller, the max SDMMC_CK frequency I can get is 40MHz ( if I enable bypass mode and I put the CLKDIV to 0 ) . Now , I'm only working with 20 MHz frequency which isn't too high I think .
2017-02-28 6:16 PM
Dear eliot,
Series resistor for impedance matching can set upto 47Ohm(must set nearby signal source).
I also use 47Ohm resistor on STM32F746G-discovery forcelly, it works well even 50MHz SDMMC Clock!
Best regards,
Nemui.
2017-04-21 12:50 AM
FYI: The issue seems to be fixed in STM32CubeF7 V1.6.1, finally.
2017-04-21 5:09 PM
Nemui,
May I ask, how/where did you install the resistor in the clock line?
Do you have a picture?
-Bill