Problem With Ethernet RMII Module Infinite SoftwareReset Loop
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-09-19 6:27 AM
Posted on September 19, 2015 at 15:27
Hello to All
I am Working on a RMII Module With DP83848v.I use Stm32f4xg Eval Board Schematic to Design this board.(you can download it in st site that you knew it better than me) i noticed that St design Ethernet that can be used as MII and RMII So i copied this Schematic to my Project(with just chnaging resistor as single resistor not Package Resistor). I assembled it in RMII Config and found that it's not Working i compare it tohttp://www.waveshare.com/w/upload/3/31/DP83848-Ethernet-Board-Schematic.pdf
from waveshare and found that pin39 in phy is connected to RX_DV_MII/CRS_DV_RMII Which is Wrong i think because in RMII CRS_DV Located in pin40.(please tell me if i'm wrong)so i cut tracks on my board and repair my board just like Waveshare's Board. i connect my ethernet module to a Stm32f429IIT Board and Connect Pins like below PA1--->MII_RX_CLK/RMII_REF_CLK PA2--->MII_MDIO PA7--->MII_CRS PC1--->MII_MDC PC4--->MII_RXD0 PC5--->MII_RXD1 PG11--->MII_TXEN PG13--->MII_TXD0 PG14--->MII_TXD1 i test module withhttps://github.com/MaJerle/stm32f429/tree/master/52-STM32F429_ETHERNET_SERVER
this project is by default RMII and i test it in another project that worked correctly and i just checked pin Configuration in GPIO_Config method. i executed project and in debug mode i see it is in an indefinite loop software reset. i checked 50MHZ MAC to phy oscilator in both end and they are OK. i replaced 10MHZ oscilator with a 8MHZ crystal(with changing programm) i used mxcube and the same result occured. i guess that long distance between ethernet module and MCU module causes problem but i'm not sure about it because 50MHZ is not a high frequency. #rmii #stm32f429
Labels:
- Labels:
-
Ethernet
-
STM32F4 Series
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-09-20 4:32 AM
Posted on September 20, 2015 at 13:32
thanks for kindness reply b:)) problem was sth relate to stm32f429 IC. i dont know why but it solves when i replace it with another chip
in some ic one peripheral is broken .i had a 407 with usb on GPIOA broken(i replaced IC so that usb worked)