2014-07-19 2:29 PM
Hi all,
I'm using the Nucleo F302R8 to build the firmware for a new board I'll develop using the same MCU. I'm trying to use USB CDC to have a VCP. I've started with CubeMX with the Nucleo F302R8 template, changed the PA11/PA12 to have USB and PF0/PF1 to have RCC_OSC (config attached) and configured the usb midleware in CubeMX. I've also soldered the solder bridges to connect the clock coming from the stlink to the stm32f3 osc_in pin (to have HSE). Did all the physical connections to an USB port but when I connect to PC it doesn't detect anything. So I guess I'm missing something. Can someone please help me? #usb #nucleof3022014-08-27 2:25 AM
Hi rodrigues.luis,
Would you mind providing the .ioc file so that we reproduce your issue.Which Nucleo board revision are you using ?Thank you.