Problem accessing Internal Boot Loader in STM32H743xx
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-11-18 6:05 AM
Hi Everyone,
I am working on a project where I need to program STM32H743xx MCU through UART, but I am facing problem in entering the internal bootloader through software. I have created a .s file to enter the bootloader where I need to wait for a firmware command and then enter the bootloader mode.
Note: I am successfully entering the bootloader mode when I directly call the DFUBoot() function but when I call through HAL_UART_RxCpltCallback I don't see any response from the bootloader.
DFU_Bootloader.s
AREA demo, CODE
PRESERVE8
ALIGN
DFU_Bootloader PROC
EXPORT DFU_Bootloader [WEAK]
IMPORT SystemInit
IMPORT __main
LDR R0, =0x2001FFFC ;
LDR R1, =0xBEEFBEEF ;
LDR R2, [R0, #0]
CMP R1, R2
BNE NotDFuse1
STR R0, [R0, #0] ; Invalidate Key
LDR R1, =0xE000ED00 ; SCB
LDR R0, =0x1FF09800 ; ROM BASE
STR R0, [R1, #8] ; VTOR
LDR SP,[R0, #0] ; ROM Stack Pointer
LDR R0,[R0, #4] ; ROM Program Counter
BX R0
ENDP
NotDFuse1 PROC
EXPORT NotDFuse1
LDR R0, =SystemInit
BLX R0
LDR R0, =__main
BX R0
ALIGN
ENDP
END
HAL_UART_Receive_DMA(&huart3,&newreceive[0],1); // UART DMA RX for firmware Cmd
// UART RX Callback
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
if(newreceive[0]==0xAA)
{
HAL_UART_Transmit_DMA(&huart3, &sendtx[0],1);
DFUBoot();
}
else{}
}
void DFUBoot(void)
{
__HAL_RCC_DMA1_CLK_DISABLE();
HAL_NVIC_DisableIRQ(DMA1_Stream0_IRQn);
HAL_NVIC_DisableIRQ(DMA1_Stream1_IRQn);
__DSB();
Boot1 = 0xBEEFBEEF; // Special Key to End-of-RAM
__DSB();
DFU_Bootloader();
}
Any help would be highly appreciated.
- Labels:
-
Bootloader
-
STM32H7 series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-11-18 7:34 AM
It is not surprising that this doesn't work from interrupt context.
Try using the method as I originally published it, or ponder how to unwind the call stack.​
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
‎2018-11-18 7:54 AM
Hi Clive,
Thank you very much for your reply. I don’t want to use reset handeler to enter Bootload mode, I need to use interrupt mode to enter bootload, Is there any other method to unwind the callback as even after disabling the DMA stream it is not working??? In STM32F4 it works in interrupt mode after remapping the memory but in STM32H7 I don’t see any register to remap. I am successful in programming STM32H7 using Hardware reset but stuct with this problem entering bootloader mode using software
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-11-18 3:38 PM
The loader is going to be intolerant to any interrupts you have functioning, this will include USART and SysTick ones, it has no understanding of what you've set up. The core also needs to unwind the NVIC state.
So setting up another DMA transaction isn't helpful. Loading the RAM constant was for the reset method. The best place to unwind would be the IRQ Handler that is firing here, and that interrupt should have the least priority. The goal being to return to the DFUBoot() function, and from there entering the system boot loader. Alternatively you can flag the request, and call DFUBoot() from the foreground task/loop.
__DSB() is rather ineffectual in the H7 caching/write-back scenario
Original method for those reader unfamiliar with it https://community.st.com/s/question/0D50X00009XkW8QSAV/stm32h743-how-to-start-the-system-boot-loader-via-software
Up vote any posts that you find helpful, it shows what's working..