2019-02-20 4:52 AM
Hi,
I want to play MP3 files that are located in an external flash.
Do I need to load the files to RAM for playing them, or can I play them directly from flash?
I'm asking because I might not have enough RAM for loading the whole file all at once.
Thanks in advance
2019-02-20 5:01 AM
The MP3 format contains packets of data, the decoder only requires on at a time. Data can be in RAM, or readable flash in the memory address space. You could also read the packets from a microSD card to RAM.