Using STM32F7 for USB Audio and HiRes Audio (DSD)
I'm looking for the appropriate MCU to include as a main processing unit in a DAC product I'm designing. The product uses an XMOS for USB Audio and is in need for a central CPU with a more approachable programming model. I came around choosing between F4 and F7, because along with user interface tasks and housekeeping, the MCU will have to handle the SPDIF/RX signal input - I'm not keen on adding S/PDIF routing into XMOS I2S routines.
I understand the F7 is substantially more powerful than the F4, so this begs the question: can I ditch the XMOS altogether and port the USB Audio Class to the F7? I mean does this part have the processing power to keep up with an audio signal that is 192k/32b?
Another tricky one: the SAI port on the F7 does not support DSD, which in it's faster iterations can go up to 11MHz on the output. Do you think it is possible to output that sort of signal out of an F7? Some designs out there use CPLDs connected to the CPU to achieve DSD, would that be the case here?
I appreciate any input on the questions here, or any interest in my project.
Thanks!