2012-08-21 6:29 AM
I was trying to add OUT report to existing HID mouse sample on STM OTG Device library 2.1.0. I am using STM3241G-EVAL.
Here are my descriptors... 0x09, /* bLength: Configuration Descriptor size */ USB_CONFIGURATION_DESCRIPTOR_TYPE, /* bDescriptorType: Configuration */ USB_HID_CONFIG_DESC_SIZ, /* wTotalLength: Bytes returned */ 0x00, 0x01, /*bNumInterfaces: 1 interface*/ 0x01, /*bConfigurationValue: Configuration value*/ 0x00, /*iConfiguration: Index of string descriptor describing the configuration*/ 0x80, //0xE0, /*bmAttributes: bus powered and Support Remote Wake-up */ 0xFA, //0x32, /*MaxPower 100 mA: this current is used for detecting Vbus*/ /************** Descriptor of custom interface ****************/ /* 09 */ 0x09, /*bLength: Interface Descriptor size*/ USB_INTERFACE_DESCRIPTOR_TYPE,/*bDescriptorType: Interface descriptor type*/ 0x00, /*bInterfaceNumber: Number of Interface*/ 0x00, /*bAlternateSetting: Alternate setting*/ 0x02, //0x01, /*bNumEndpoints*/ 0x03, /*bInterfaceClass: HID*/ 0x00, //0x01, /*bInterfaceSubClass : 1=BOOT, 0=no boot*/ 0x00, //0x02, /*nInterfaceProtocol : 0=none, 1=keyboard, 2=mouse*/ 0, /*iInterface: Index of string descriptor*/ /******************** Descriptor of custom HID ********************/ /* 18 */ 0x09, /*bLength: HID Descriptor size*/ HID_DESCRIPTOR_TYPE, /*bDescriptorType: HID*/ 0x11, /*bcdHID: HID Class Spec release number*/ 0x01, 0x00, /*bCountryCode: Hardware target country*/ 0x01, /*bNumDescriptors: Number of HID class descriptors to follow*/ 0x22, /*bDescriptorType*/ HID_MOUSE_REPORT_DESC_SIZE,/*wItemLength: Total length of Report descriptor*/ 0x00, /******************** Descriptor of IN endpoint ********************/ /* 27 */ 0x07, /*bLength: Endpoint Descriptor size*/ USB_ENDPOINT_DESCRIPTOR_TYPE, /*bDescriptorType:*/ HID_IN_EP, /*bEndpointAddress: Endpoint Address (IN)*/ 0x03, /*bmAttributes: Interrupt endpoint*/ HID_IN_PACKET, /*wMaxPacketSize: 64 Byte max */ 0x00, 0x0A, /*bInterval: Polling Interval (10 ms)*/ /* 34 *///********************Descriptor of OUT endpoint ********************/ 0x07, /* bLength: Endpoint Descriptor size */ USB_ENDPOINT_DESCRIPTOR_TYPE, /* bDescriptorType: */ HID_OUT_EP, /* bEndpointAddress: Endpoint Address (OUT) */ 0x03, /* bmAttributes: Interrupt endpoint */ HID_OUT_PACKET, /* wMaxPacketSize: 64 Bytes max */ 0x00, 0x0A, /* bInterval: Polling Interval (1 ms) */ /* 41 */ And report descriptor is as follows : [ 0x06, 0x00, 0xff, // USAGE_PAGE (Vendor Defined Page 1) 0x09, 0x01, // USAGE (Vendor Usage 1) 0xa1, 0x01, // COLLECTION (Application) // ------ common globals ------ 0x15, 0x00, // LOGICAL_MINIMUM (0) 0x26, 0xff, 0x00, // LOGICAL_MAXIMUM (255) 0x75, 0x08, // REPORT_SIZE (8) - bits // ------ input report ------ 0x95, 0x40 // REPORT_COUNT - bytes 0x09, 0x01, // USAGE (Vendor Usage 1) 0x81, 0x02, // INPUT (Data,Var,Abs) // ------ output report ------ 0x95, 0x40, // REPORT_COUNT - bytes 0x09, 0x01, // USAGE (Vendor Usage 1) 0x91, 0x02, // OUTPUT (Data,Var,Abs) 0xc0 // END_COLLECTIONAnd added the Data out funcxtion as follows :static uint8_t USBD_HID_DataOut( void *pdev, uint8_t epnum ){ if ( epnum != (HID_OUT_EP & 0x0F) ) return USBD_FAIL; /* Get the received data buffer and update the counter */ pointertoUSBPACKET = ((USB_OTG_CORE_HANDLE*)pdev)->dev.out_ep[epnum].xfer_count; //try to send it back... //USBD_HID_SendReport (&USB_OTG_dev,USBPACKET,pointertoUSBPACKET); /* Prepare Out endpoint to receive next packet */ DCD_EP_PrepareRx(pdev, HID_OUT_EP, (uint8_t*)(USBPACKET), HID_OUT_PACKET); return USBD_OK;}My device succesfully enumerates, but i can not read/write reports.I am trying to send the reports from SysTick_Handler.The problem is when i try to get report/set report using SimpleHIDWrite, it always fails with ''A device attached to the system is not functioning'' (1F)Another thing i noticed if i try to write using SimpleHIDWrite and first byte is 0 then i get the control in USBD_HID_DataOut() but pointertoUSBPACKET always gets 0. And if i change the first byte to anything other than 0 it always fails with ''Parameter is incorrect (57)''. So in report descriptor do we need to have the Report IDs , is it mandatory?Please give me some pointers, thanks #usb #hid #custom-usb-hid