cancel
Showing results for 
Search instead for 
Did you mean: 

mDNS on LWIP TCP server

jaykay
Associate

I'm tying to setup TCP server using ethernet communications (Nucleo-F767ZI) and find that I can ping the board using the router allocated IP address but I'd like to do the same using Hostname. In STM32CubeMx .ioc file, under Network Interface Options, LWIP_ENABLE_NETIF_HOSTNAME is set to 'enable' and I've set the host name I want to use in LWIP_NETIF_HOSTNAME to 'my_lwip'. However, I still find that I cannot ping the board using the hostname. I know my router DNS is working Ok because I can ping a Raspberry Pi using it's host name.

I realize that in STM32CubeMX generated lwipopts.h #define LWIP_NETIF_HOSTNAME is set to my_lwip by default but I change this to 1 manually. Otherwise, in ethernetif.c, the statement netif ->hostname - "my_lwip" is not enabled.

I think mDNS has to be enabled in LwIP. However, under MDNS/TFTP tab in CubeMX, LWIP_MDNS is always disabled and there is no enable option in the drop-down list.  I've seen a post that suggests to enable LWIP_MDNS, LWIP_UDP and LWIP_IPV4_IGMP have to be enabled.  However, I find that LWIP_IPV4_IGMP has the same issue i.e. no enable option in the drop-down list.   Has anybody successfully enabled mDNS? Thanks.

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
Andrei Chichak
Lead II

The zip file that was attached (above) does in fact work. The host name configured in the .ioc file gets converted by the mDNS system into "nicehostname.local".

It  takes a while for the name to propagate though. I could not ping my board for around a minute before the name resolution took effect.

The project is an HTTP server as well. You can point your browser to nicehostname.local and it shows a default LwIP splash screen.

If you were to add the line:

mdns_resp_add_service(&gnetif, "Nucleo-144 demo server", "_http", DNSSD_PROTO_TCP, 80, 60, srv_txt, NULL);

after the mdns_resp_add_netif line, then your board will be advertised with the other http servers on your local network. You can use programs like "Discovery" for MacOS to see this in action.

View solution in original post

7 REPLIES 7
STea
ST Employee

Hello @jaykay ,

In order to make this work here are the steps you should follow:

Make sure to display the help for each LWIP option in CubeMX, using the round "i" button, and note that in some panels there is a "Show advanced parameters" checkbox which may need to be activated in case the required parameter is hidden by default.

To enable mDNS: * Under key options, enable LWIP_MULTICAST_TX_OPTIONS *

Under general settings, enable LWIP_IGMP *

Now in the mDNS/TFTP tab, it should be possible to enable mDNS It may be necessary to also show the advanced options in the mDNS tab and enable LWIP_MDNS_RESPONDER.
note that IGMP flag doesn't get set directly from MX and should be done manually in previous version of MX and it will be fixed in upcoming revisions.
you will find attached the IOC file with proper configuration for mDNS.
Regards 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi @STea 

 

I'm trying to do the same thing to resolve my my IP via hostname and I could not achieve the same.

I followed the steps you mentioned.

I could ping my device via the IP attained through DHCP but not through hostname. Looks like the default is set as "lwipW . I tried to ping lwip and lwip.local

surendersampath_0-1730466163763.png

I also override the 

surendersampath_1-1730466307681.png

 

Attached my ethernet.ioc in case if you take a look and help me please.

 

 

 

 

Hello @surendersampath ,

you will find attached the project in which MDNS and all configurations needed where done.

if you are trying to test with direct connection from board to pc this should be done.

added mdns_resp_init(); in MX_LWIP_init() 

and 

in while(1) of main.c		
if(dhcp_supplied_address(&gnetif))
		{
			mdns_resp_add_netif(&gnetif, gnetif.hostname, 60);
			validadd = 1;
		}

Regards

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello @STea 

I have tried the solution you sent but still cannot ping using host name.  In my setup, I've connected the PC and NUCLEO-F767ZI to a Netgear 300 router.  I can ping using the allocated IP address (as seen via TeraTerm) but not the hostname.  Perhaps you can share your test setup?

Regards.

Andrei Chichak
Lead II

The zip file that was attached (above) does in fact work. The host name configured in the .ioc file gets converted by the mDNS system into "nicehostname.local".

It  takes a while for the name to propagate though. I could not ping my board for around a minute before the name resolution took effect.

The project is an HTTP server as well. You can point your browser to nicehostname.local and it shows a default LwIP splash screen.

If you were to add the line:

mdns_resp_add_service(&gnetif, "Nucleo-144 demo server", "_http", DNSSD_PROTO_TCP, 80, 60, srv_txt, NULL);

after the mdns_resp_add_netif line, then your board will be advertised with the other http servers on your local network. You can use programs like "Discovery" for MacOS to see this in action.

Hey @STea I have some more information regarding mDNS.

If you were to run the HTTP_Server project, you'll notice that the mDNS announcement will disappear after a while.

The announcement  is set up with a time-to-live value of 60 seconds and when the devices on my LAN stop asking, the announcement expires. It's usually in the 2 hour range, but the mDNS system just never refreshes the announcement.

After much messing about I found a random GitHub discussion in the ESP32 community explaining a workaround where, before the TTL expires, you 

mdns_resp_del_service(netif, serviceSlot);

and then re-add the service

static s8_t serviceSlot;

serviceSlot = mdns_resp_add_service(&netif, hostNameString, PATCH_SERVICE_NAME, DNSSD_PROTO_TCP, PATCH_PORT, MDNS_TTL, GetServiceText, NULL);

 So far, my announcement has been valid for 22.4 hours whereas it would normally die in a time frame of minutes to  a few hours.

I have no expectation that this will get fixed in LwIP, or even that someone will explain how mDNS refresh SHOULD be done according to the design. mDNS in LwIP seems to be a throw-away piece that nobody is supporting, developing, or using, even though it is extraordinarily useful.

Anyway, I thought I'd leave a note for others that run into this issue in the future, so they don't give up or duplicate my work.

Hello @Andrei Chichak,

Thanks a lot for sharing this with the community members. this should save lots of hours for another user when using this feature.
Regards

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.