cancel
Showing results for 
Search instead for 
Did you mean: 

LwIP: set IP address, mask, and Gateway address of stm32 remotely

abeba.1
Associate III

hii every one 

 

i have a question about setting up the ip of the STM32 MCU remotely 

 

when we want to do client server in udp or tcp on stm32 controller , we are used to set the ip address manually in the ioc file in general settings in the lwip section in the middleware tab .

 

and i was wondering if there is a way to set up any default ip of mine , and is there a way to change this ip remotly after i am connected to the stm32 .

 

my goal is to design an application that can give me the ability to access and change the ip and mask and gateway of my stm32 controller , i be very thankful for help and to know if there is a method to do that  

24 REPLIES 24

@abeba.1 wrote:

is applying the setting  with the appropriate APIs to your network stack require me to compile the project  


No.

it might require a reset - check with the stack documentation.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

hii Andrew thanks for help it helped me a lot 

 

thats my code of the lwip_init () in the lwip.c


/**
* LwIP initialization function
*/
void MX_LWIP_Init(void )
{


/* IP addresses initialization */
IP_ADDRESS[0] = 192;
IP_ADDRESS[1] = 168;
IP_ADDRESS[2] = 127;
IP_ADDRESS[3] = 100;
NETMASK_ADDRESS[0] = 255;
NETMASK_ADDRESS[1] = 255;
NETMASK_ADDRESS[2] = 255;
NETMASK_ADDRESS[3] = 0;
GATEWAY_ADDRESS[0] = 0;
GATEWAY_ADDRESS[1] = 0;
GATEWAY_ADDRESS[2] = 0;
GATEWAY_ADDRESS[3] = 0;

/* USER CODE BEGIN IP_ADDRESSES */
/* USER CODE END IP_ADDRESSES */

/* Initialize the LwIP stack without RTOS */
lwip_init();

/* IP addresses initialization without DHCP (IPv4) */
IP4_ADDR(&ipaddr, IP_ADDRESS[0], IP_ADDRESS[1], IP_ADDRESS[2], IP_ADDRESS[3]);
IP4_ADDR(&netmask, NETMASK_ADDRESS[0], NETMASK_ADDRESS[1] , NETMASK_ADDRESS[2], NETMASK_ADDRESS[3]);
IP4_ADDR(&gw, GATEWAY_ADDRESS[0], GATEWAY_ADDRESS[1], GATEWAY_ADDRESS[2], GATEWAY_ADDRESS[3]);

/* add the network interface (IPv4/IPv6) without RTOS */
netif_add(&gnetif, &ipaddr, &netmask, &gw, NULL, &ethernetif_init, &ethernet_input);

/* Registers the default network interface */
netif_set_default(&gnetif);

/* We must always bring the network interface up connection or not... */
netif_set_up(&gnetif);

/* Set the link callback function, this function is called on change of link status*/
netif_set_link_callback(&gnetif, ethernet_link_status_updated);

/* USER CODE BEGIN 3 */

/* USER CODE END 3 */
}

 

this function is generated automatically when is disable dhcp in the ioc file as yo can see the ip that is configured is 192.168.127.100

 

lets say i want to set a new ip that is received from uart  as a side channel and the new ip for example will be 

192.168.127.103

 

what functions do i need  to use in order to update the new ip address into the network interface 

 

from my understanding i need the following steps to do after a bit of research:

1- to use the macro IP4_ADDR to initialize the new ip address netmask and gateway without dhcp  

2- add the network interface using netif_add

3-and somehow to trigger or call a function that do the update to the network interface i am using stmcube ver 1.17.2 what is the function that does this update ?

 

another question do i need to create a function that does all 1-3 operations?

and did i mess something? another operation that needs to be added ?

 

and where is the place to put this operations in what file lwip.c or main.c ?

where is the most appropriate once i get the new ip in the uart 

 

i forget one question also is there a function that does some kind of restart  to bring the network interface down and bring it up at the end of the operations sort of reboot 

Please see: How to insert source code.

 


@abeba.1 wrote:

what functions do i need  to use in order to update the new ip address into the network interface 


you need to see the LwIP documentation for that.

It's a widely-used 3rd-party stack - not specific to STM32.

https://savannah.nongnu.org/projects/lwip/

 


@abeba.1 wrote:

do i need to create a function that does all 1-3 operations?


It doesn't matter how you do them - so long as they get done!

 


@abeba.1 wrote:

and where is the place to put this operations in what file lwip.c or main.c ?


As with any C code, It can be in any file you like - It really doesn't make any difference to the operation!

 

PS:

https://www.google.com/search?q=lwip+change+ip+address+runtime 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

hii thanks for help i will try to set the ip network down before it and will try one more time