2023-07-10 8:59 AM
Hello,
I am setting up just a simple task with a timer in CMSIS V.2 that triggers a periodic call of a callback function.
Despite the fact that I am including "cmsis_os.h", which is part of my project, I get the linker error "undefined reference to `osTimerCreate'".
Does anybody have an idea other than "switch to CMSIS V.1"?
Thanks in advance
Wilfried
2023-07-10 9:20 AM
An include file typically ISN'T CODE, it describes the interface expectations, find the file with the backing source code for the function, and add that to the project.
2023-07-10 10:57 AM
thanks, Tesla DL, but the root of the problem was that I was mislead to CMSIS 1, when I was googling for osTimerDef at Keil. The 'osTimeCreate' function was replaced by 'osTimeNew' in CMSIS 2.
Thanks for your willingness to support,
Wilfried