Skip to main content
PM.5
Associate III
October 18, 2023
Question

LCD TFT display interface with Spi to Stm32h745i disco

  • October 18, 2023
  • 2 replies
  • 1209 views

Hi,

I am using STM 32H745I disco boards. When I have configured the boards with LTDC interface image has been displayed on 480*272 display.

Now we have removed on board 480*272 display , we have connected external 480*480 display & I have initize the display through SPI.

I want to know wheather is it possible ? 

If yes ...then how it needs to be configured ?

Thankyou 

This topic has been closed for replies.

2 replies

TDK
October 18, 2023

The datasheet of the display should tell how to use it. If it doesn't connect over LTDC, you're going to need a different interface to control it compared to the previous display.

"If you feel a post has answered your question, please click ""Accept as Solution""."
EXUE.2
ST Employee
November 3, 2023

so what is the question?

I understand your mean is that 1. you used LTDC to connect 480*272 display before; 2. now you want to use SPI to connect 480*480 display?

if the display support the SPI interface, it is possible to apply this display on board, but the image transfer speed will be lower than LTDC interface.